MCAT for two motors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCAT for two motors

1,090 Views
peterkostadinov
Contributor III

Hi All,

I'm using an example project from "MCRSP_PMSM_V1.2.0" and also FreeMaster+MCAT "pmsm_ref_sol.pmp". For my application I need to handle parameters for two PMSM motors in one FreeMaster+MCAT project. According to the datasheets it is possible, but in "pmsm_ref_sol.pmp", the motor selector bar is missing. 

Best Regards,

Peter

0 Kudos
Reply
2 Replies

953 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Peter,

 

You may want to take a look to the following application note, it could give you an idea of how to implement it.

Dual Motor Control for PMSM with the Kinetis K70

 

Please find code attached.

 

Best regards,

Felipe

0 Kudos
Reply

953 Views
peterkostadinov
Contributor III

Hi Filipe,

Thank you very much for the information provided. Your answer is not exactly related to my question about 2 motors in one FreeMaster + MCAT project (see the picture below), but it still gives me very valuable guidance in my work.

Untitled.png

Best Regards,

Peter

0 Kudos
Reply