Is there any multi-motor example based on MCRSP_PMSM?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there any multi-motor example based on MCRSP_PMSM?

1,136 次查看
ristomustonen
Contributor II

I am testing MCRSP_PMSM_V1.2.0 motor control package (twrkv58f) and it works fine with one BLDC motor. There are lots of references about M1 (motor 1) on that example. I wonder if there is some example for dual motor solution with this package and KV58 platform?

Thank's Risto.

标记 (1)
0 项奖励
2 回复数

834 次查看
philip_drake
NXP Employee
NXP Employee

I could recommend quad BLDC on KV4x used for Drone ref. design.

https://www.nxp.com/support/developer-resources/reference-designs/quadcopter-drone-reference-design:...

https://www.nxp.com/webapp/Download?colCode=AN5169-SOFTWARE

The KV4 and KV5 are both capable of running 4 BLDC motors.  The KV11 can run two BDLC motors, The KV4 has enough timers and a fast enough ADC to do two PMSM FOC motors.

  

Regards,

Philip

0 项奖励

834 次查看
ristomustonen
Contributor II

Hi, Philip!

All right! That will be a good ref. design. Thank you for the recommendation.

BR,

Risto

0 项奖励