channel id error for dio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

channel id error for dio

ソリューションへジャンプ
135件の閲覧回数
Esakki
Contributor II

Hello nxp team,

we are trying to enable the PTD17 pin high with dio peripheral

port name: PTD_H

Dio port Id: 7

Dio channel Id: 1

how to check the channel id i set is correct or not?

right now this pin is not getting high.

ラベル(1)
0 件の賞賛
返信
1 解決策
66件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hi @Esakki 

For achieving a correct configuration of PTD17 inside the Dio component, could you please check the following article (link)? It provides a complete description of the mapping between the Port Id, Channel Id and the pin that should be configured.

The article also presents a demo application, showcasing how certain values can be written to the pins, or how the pins values can be read, using the APIs exposed by the MBDT Dio Simulink block.

Hope this helps,

Irina

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
67件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hi @Esakki 

For achieving a correct configuration of PTD17 inside the Dio component, could you please check the following article (link)? It provides a complete description of the mapping between the Port Id, Channel Id and the pin that should be configured.

The article also presents a demo application, showcasing how certain values can be written to the pins, or how the pins values can be read, using the APIs exposed by the MBDT Dio Simulink block.

Hope this helps,

Irina

0 件の賞賛
返信