HotFix: MBD Toolbox rev1.3.0 for MPC564xL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HotFix: MBD Toolbox rev1.3.0 for MPC564xL

2,563 次查看
paulvlase
NXP Employee
NXP Employee

HotFix_1: Fix "Undefined function 'slsfnagctlr'..." when trying to generate code on R2016b/R2017a

 

NXP Tracking number: AST-527

 

Problem: If you try to generate code for any model on R2016b/R2017a, you will receive this error: "Undefined function 'slsfnagctlr' for input arguments of type 'char'." 

 

Root Cause: Matlab API change.

 

Workaround:  Update the files attached in the following folders 

{Toolbox install dir}\rappid564xl\rappid564xl\mscripts folder slsfnagctlr.p file

 

Customer Report: BUG report

Special thanks to Michael Verrecchia for reporting this issue.

标签 (1)
标记 (1)
4 回复数

1,693 次查看
paulvlase
NXP Employee
NXP Employee

HotFix_2: Fix license errors for DISK_SERIAL_NUM with less than 8 characters

NXP Tracking numberAST-619

 

Problem: If your HDD has a serial number with less than 8 characters, the license checking and validation will fail even if the license is correctly generated

 

Root Cause: Coding logic error

 

Workaround:  Update the rappid_hostid.p file attached in the following folder 

{Toolbox install dir}\rappid564xl\rappid564xl\mscripts

 

Customer Report: Undefined function or variable 'lic_err'.

0 项奖励

1,693 次查看
jjacp
Contributor III

Hi paulvlase‌,

Is this fix available for the MBD v2.0.0 Toolbox for the MPC5744P (Panther)? I'm running R2018a and am getting the slsfnagctlr error.

Thanks!

0 项奖励

1,692 次查看
constantinrazva
NXP Employee
NXP Employee

Hello jjacp‌,

Yes, there is a fix available for Panther (MPC5744P). I have attached it here.

Please move slsfnagctlr.p file into 

   {TOOLBOX_TOOL_ROOT}\mbdtbx_pnt\mbdtbx_pnt\mscripts

Kind regards,

Razvan.

1,692 次查看
jjacp
Contributor III

Thanks constantinrazvan.chivu! It works!

0 项奖励