HotFix: MBD Toolbox 3.0.0 for MPC57xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HotFix: MBD Toolbox 3.0.0 for MPC57xx

3,255 次查看
mariuslucianand
NXP Employee
NXP Employee

HotFix_1: eTimer pins initialization not working properly, added support for ADC internal temperature sensor.

 

Problem: When using other port than PORTA on eTimer input channels, the initialization was not performed right.

 

Root Cause: eTimer input pins not working on other ports than PORTA.

 

Usage: Run MBDT_MPC57xx_patch_1.exe and enter the following path when prompted:

{YOUR_INSTALL_DIR}\NXP_MBDToolbox_MPC57xx\code

e.g.: C:\Users\my_user_name\Documents\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_MPC57xx\code

Most likely you will be asked if you want to overwrite some files - just click on 'Yes to All' option. 

Special thanks to abhishek.kumar@chassisbrakes.com‌ for reporting the eTimer issue and requesting the ADC internal temperature support.

标签 (1)
5 回复数

2,444 次查看
462150318
Contributor I


Hello engineers,

I am facing a problem when i excute the code as  shown in  https://community.nxp.com/message/964538.

The code can be download but  does not executing on MPC5744P DevKit. Is there a solution? PS : I use matlab 2018a and mbd toolbox 3.0.0.

Thanks very much and wait for your reply!

0 项奖励
回复

2,444 次查看
constantinrazva
NXP Employee
NXP Employee

Cumulative patch:

 

As you know, we're only giving out cumulative patches for a while now - they come in the form of self-extracting zips and contain all the patches, up-to-date. A user can install at any point in time the latest patch and get all the patches from before, regardless if he had or had not installed some previous patch.

 

Usage:

 

Run MBDT_MPC57xx_patch_2.exe and enter the following path when prompted:

{YOUR_INSTALL_DIR}\NXP_MBDToolbox_MPC57xx

e.g.: C:\Users\my_user_name\Documents\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_MPC57xx

Note: for older versions of MATLAB, you might have the toobox installed in {ROOT}\NXP_MBDToolbox_MPC57xx\code . If you have the 'code' folder generated, you must add that path. 

 

Most likely you will be asked if you want to overwrite some files - just click on 'Yes to All' option. This is an indicator of things going ok. If you do not get such a prompt, something is wrong with the patch / path given.

 

MBDT_MPC57xx_patch_2 contains:

  • HotFix1 - eTimer pins initialization issue
  • HotFix2 - RevE RBF added
  • HotFix3 - CAN Receive individual masking not working as expected
  • HotFix4 - SPI - not all CS available

 

As we get more fixes in, we'll update both the list and the executable file you need to install here.

2,444 次查看
constantinrazva
NXP Employee
NXP Employee

HotFix_3: CAN Receive individual masking not working as expected

 

Problem: When using CAN Receive block, individual masking is not enabled

 

Root Cause: Reset value of MCR[IRMQ] is 0 - global masking enabled;

 

Workaround:  Update the following file:

{ROOT_DIR}\mbdtbx_mpc574x\mbdtbx_mpc574x\blocks\fcan\fcan_mpc574x_receive.tlc

which enabled individual masking for MBs.

 

Customer Report: 

Special thanks to aungkm@outlook.com‌ for reporting this issue.

0 项奖励
回复

2,444 次查看
constantinrazva
NXP Employee
NXP Employee

HotFix_4: SPI - not all CS available

 

Problem: Only CS0 through CS3 available

 

Root Cause: Oversight - some instances have 0-3, others 0-7 available.

 

Workaround:  Update the following files:

{ROOT_DIR}\mbdtbx_mpc574x\mbdtbx_mpc574x\mbd_mpc574x_ec_toolbox.mdl
{ROOT_DIR\mbdtbx_mpc574x\mbdtbx_mpc574x\mscripts\spi\mbd_mpc574x_spi_instance_callback.p

 

Customer Report: 

Special thanks to Abhishek Kumar for reporting this issue.

2,444 次查看
mariuslucianand
NXP Employee
NXP Employee

HotFix_2: New board design (Rev E) for MPC5744P EVB

 

Problem: The existing Bootloader rbf file will not deploy code on the target because the UART pins were changed from PD9/PD12 to PB2/PB3

 

Root Cause: Hardware changed

 

Usage: Flash the attached .rbf bootloader on the Rev E  board in order to program the board using the OpenSDA and RappId bootloader. 

Special thanks to aungkm@outlook.com‌ for reporting this issue on our Community.

0 项奖励
回复