FreeMaster not connecting over CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeMaster not connecting over CAN

1,298 Views
mahdkhalid
Contributor III

Hi Dear dumitru-daniel.popa

I have attached the files which I built using my compiler. Please have a look.

Many thanks in advance,

Mahd

2 Replies

1,050 Views
mahdkhalid
Contributor III

Hi dumitru-daniel.popa‌,

Thank you so much for your help.

I have installed hotfix_6 and everything is working totally fine now

Best regards,

Mahd Khalid

0 Kudos
Reply

1,050 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Mahd, 

Sorry for delay. I've checked the code you have sent me.

The main difference between you generated code and mine is in the flexcan_init_fnc() function:

pastedImage_1.png

Please install HotFix_6 patch in order to fix it: https://community.nxp.com/thread/451804#comment-954427 

This is a cumulative patch that fix the issue.

Please confirm you have it working. FYI, these are the HW settings i've tested with:

- 12V external power supply

- 120ohm termination resistor

pastedImage_3.png

Hope this helps!

Daniel