Can you do external mode and PIL for all sets of JTAG pin counts?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can you do external mode and PIL for all sets of JTAG pin counts?

314 Views
Poley
Contributor V

Hi all,

 

I am currently designing a new board and will want to carry out PIL testing from the simulink blockset but there is multiple versions of JTAG pins. Do I need to have a certain configuration? I am using a S32K144 and the evaluation board for that shows a 10 pin version but the S32K148 EVB shows a 20 pin version. What one do I need to be able to run PIL and external mode through a JTAG device? Obviously 10 pin is preferable for less tracks and pins.

 

Poley_0-1680943409033.png

 

 

Thanks!

0 Kudos
0 Replies