Can FD example for HVBMS S32K344

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can FD example for HVBMS S32K344

1,017 次查看
yassinechamam
Contributor III

Hi,

we are trying to connect the RD-K344BMU with RD33775ACNCEVB using the CAN FD. i am successfully debugging the hvbmu2_775a_read_s32ct on the board but as i understand from freemaster the TDEncoding is using TPL and not the CAN. How can i change the setup of the Model for it to use CAN and not TPL or is there a Project that is already made for CAN. 

标签 (1)
标记 (3)
0 项奖励
回复
0 回复数