Why is the CRC driver removed from MQX 4.1.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why is the CRC driver removed from MQX 4.1.0

跳至解决方案
686 次查看
chrissolomon
Contributor III

Hi,

I am in the process of update our product to use MQX 4.1, from 4.0.1.

We have been using the CRC driver provided in MQX (mqx/source/io/crc), but it seems to be missing in MQX 4.1.0.

For the moment I have copied the crc driver (having updated the types to C99) into our application.

Can I ask why this is?

Is there a problem with the hardware CRC module in the K70?

Should we not use it?

Thanks

Chris

标记 (5)
0 项奖励
回复
1 解答
428 次查看
RadekS
NXP Employee
NXP Employee

No, there isn’t any problem with hardware CRC module.

CRC driver was removed from official release just due to platform dependency.

You can use CRC driver from MQX 4.0.1 (after types update).


Best Regards,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
429 次查看
RadekS
NXP Employee
NXP Employee

No, there isn’t any problem with hardware CRC module.

CRC driver was removed from official release just due to platform dependency.

You can use CRC driver from MQX 4.0.1 (after types update).


Best Regards,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复