Why is "IO_IOCTL_CHAR_AVAIL" only working when receiving 1 byte (UART)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why is "IO_IOCTL_CHAR_AVAIL" only working when receiving 1 byte (UART)

650件の閲覧回数
m4l490n
Contributor V

Hello

I have a project where I use my board's UART4 with the stdio and I can "printf" just fine. Additionally, I need that very same port for another part of my project so in my code I open it with:

port = fopen("ttye:", IO_SERIAL_RAW_IO);

That works wonderfully because I can send data through the port using:

write(port, data, size);

But I'm having some problems when reading bytes from the port. I found a post where someone has a similar case scenario than me and wants to find out when four bytes have arrived into the port. Nevertheless, the post is 5 years old and inconclusive since it does not have a satisfactory answer and it doesn't help my situation.

It is suggested in the post to use "IO_IOCTL_CHAR_AVAIL" to detect bytes available. I'm doing it like this:

ioctl(port, IO_IOCTL_CHAR_AVAIL, &result);

But the problem is that I only get TRUE if the reception is 1 byte only and I need to detect when more than 1 byte has arrived.

Why is this happening? Or is there any other way of detecting when more than one bytes have been received?

By the way, I can't use interrupts and it's ok to poll as I'm doing it right now. And I can't use "fread" because that blocks execution even if I open the port with "IO_SERIAL_NON_BLOCKING".

I don't know if I'm facing these problems because of the fact that I'm trying to use the same port as the stdio, but I can write just fine to the port using printf and write. Isn't it the same for the reception?

Thanks!

タグ(3)
0 件の賞賛
1 返信

572件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi  Manuel:

See below lines for the usage of IO_IOCTL_CHAR_AVAIL.

do {
            if (IO_OK != ioctl(f_uart, IO_IOCTL_CHAR_AVAIL, &ch_avail)) {
                printf("\nUnexpected error occured");
                _task_block(); /* unexpected error occured */
            }
            if (ch_avail == TRUE) {
               /* read data from UART */
               num_done = fread(uart2usb + uart2usb_num, sizeof(uart2usb[0]), 1, f_uart); /* read max. 1 character from UART */
               if (IO_ERROR == num_done)
               {
                  printf("\nUnexpected error occured");
                  _task_block(); /* unexpected error occured */
               }
               uart2usb_num += num_done;
            }
         } while ( (ch_avail == TRUE) && (uart2usb_num < (sizeof(uart2usb)

You can call  _time_delay() to allow lower priority tasks to run.

Regards

Daniel

0 件の賞賛