Where to place the right path?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to place the right path?

500 Views
frankdeleeuw
Contributor I

KDS keeps missing the location of MGX_cnfg.h while building a standard example:

c:\freescale\ksdk_1.2.0\platform\osa\inc\fsl_os_abstraction_mqx.h:83:22: fatal error: mqx_cnfg.h: No such file or directory

#include "mqx_cnfg.h"    (and this x22.)

and as it is the last error, I tried to add the full directory to several positions in the Project-Properties and in Window-Preferences, to no avail.

Which way to make it find it?

-Frank

Labels (2)
0 Kudos
Reply
1 Reply

366 Views
soledad
NXP Employee
NXP Employee

Hello Frank,

Unfortunately I can not to reproduce you issue. Could you please let me know which example and device are you using?

Did you build the ksdk_mqx_lib_<board>, mqx_stlib_<board> and mqx_<board> libraries?

Regards

Soledad

0 Kudos
Reply