Hello MQX community,
I am new to MQX and I am trying to find MQX example for USB keyboard device. I found the example for USB Keyboard host. Is there any example which has USB keyboard device implemented?
If the example doesn't exist, could anyone show me the closest matching example of any other device that I could make use of?
Thanks in advance!
Hi Omkar:
Please refer to the USB keyboard example in the MQX installation folder, including host and device.
C:\Freescale\Freescale_MQX_4_2\usb_v2\example\device\hid\hid_keyboard
C:\Freescale\Freescale_MQX_4_2\usb_v2\example\host\hid\keyboard
Regards
Daniel
Hello,
I am trying to port USB Keyboard example to my running application which uses MQX 4.0.0.2 version. I can't upgrade the RTOS to 4.2.0 at this point. What is the best way to port the hid_keyboard example from MQX 4.2.0 to MQX 4.0.0.2?
Could you provide some guideline?
Thanks!
USB v2 is a new unified USB stack, is designed to replace the legacy usb stack in MQX RTOS. It is possible to be ported to MQX 4.0 if you don't want to upgrade the RTOS. I would suggest you take a look at the USB_Stack_Porting_User_Guide under the MQX installation folder.
Freescale_MQX_4_2\doc\usb_v2\USB_Stack_Porting_User_Guide.pdf
Regards
Daniel
According to stack porting user guide mentioned here, I need to port fsl_usb_ehci_hal.h file or fsl_usb_khci_hal.h file but it is not mentioned where to. I tried copying whole usb_v2 folder along with the old MQX RTOS 4.0.0 but after all hustles of compilation errors and warnings I got following linking error
Error[Li005]: no definition for "USB_Framework_Periodic_Task" [referenced from usb_class.o(libusbd_mqx.a)]
I tried defining particular pre-processor directives but still can't get rid of this linking error. I have tried everything I could possibly think of.
Does anyone have USB Keyboard example for MQX RTOS 4.0.0? Please provide some guideline.
Thanks!
Omkar Karmalkar