I am using a K60
I do not understand why I am getting an Unhandled Exception for a vector I have installed a handler for!
I am using a pin on PortE and initialize as follows:
#ifdef __MQX__ if (!lwgpio_init(&fpga_irq, BSP_FPGA_IRQ, LWGPIO_DIR_INPUT, LWGPIO_VALUE_NOCHANGE)) { sprintf(zarr, "Error opening FPGA IRQ %d\r\n", _task_errno); MON_PRINTF(zarr); _task_block(); } lwgpio_set_functionality(&fpga_irq, 1); // MUX=1 is GPIO lwgpio_set_attribute(&fpga_irq, LWGPIO_ATTR_PULL_UP, LWGPIO_AVAL_ENABLE); if (!lwgpio_int_init(&fpga_irq, LWGPIO_INT_MODE_FALLING)) { MON_PRINTF("Initializing button GPIO for interrupt failed.\n"); _task_block(); }
/* install gpio interrupt service routine */ _int_install_isr(lwgpio_int_get_vector(&fpga_irq), FPGA_lisr, (void *) &fpga_irq); /* set the interrupt level, and unmask the interrupt in interrupt controller*/ _bsp_int_init(lwgpio_int_get_vector(&fpga_irq), 3, 0, TRUE); /* enable interrupt on GPIO peripheral module*/ lwgpio_int_enable(&fpga_irq, TRUE); #endif
And my ISR looks like this:
VOID FPGA_lisr(void *pin) { FPGA_QUEUE_MSG msg;
lwgpio_int_clear_flag((LWGPIO_STRUCT_PTR)pin);
/* do stuff and send message (maybe) and return */
msg.type = FPGA_IRQ; msg.arg[0] = HS_Flags; msg.arg[1] = IDLE_Flags; msg.arg[2] = pm_last_lisr; msg.arg[3] = pm_last_lisr; _lwmsgq_send(fpga_queue, (uint32 *)&msg, 0); }
The interrupt does work but in short order I find myself getting a task exception set in _int_default_irs
I have a breakpoint set there and the vector is the same as the one I installed the handler for.
What could cause that?
Tom
已解决! 转到解答。
Hi Tom, Please be very careful when _lwmsgq_send used in the ISR.
1, If LWMSGQ_SEND_BLOCK_ON_FULL set, then _task_block maybe called.
2. If LWMSGQ_SEND_BLOCK_ON_FULL not set but the MSGQ is full, the function will fail with LWMSGQ_FULL.
I would like suggest that
1. Just sent a event to a task in the ISR.
2. Send the msg in the task.
Hi Tom, Please be very careful when _lwmsgq_send used in the ISR.
1, If LWMSGQ_SEND_BLOCK_ON_FULL set, then _task_block maybe called.
2. If LWMSGQ_SEND_BLOCK_ON_FULL not set but the MSGQ is full, the function will fail with LWMSGQ_FULL.
I would like suggest that
1. Just sent a event to a task in the ISR.
2. Send the msg in the task.