USB MSD on K20

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB MSD on K20

697件の閲覧回数
derekdrost
Contributor III

Hello everyone,

     I am working on setting up a USB MSD on an MK20DX256VMD10.

     I am using the default example in mqx. (MQX_ROOT>usb>device>examples>msd>disk>cw10).

     When connected to a PC, it connects, but it comes up as an unknown device.

     Any thoughts on what could cause this?

Thank you,

Derek

0 件の賞賛
2 返答(返信)

416件の閲覧回数
derekdrost
Contributor III

I am using the correct cable. I am not using a freescale board however.

Looking over the schematics, the hardware looks to be set up correctly. Could there be something in my clocks that might be off?

0 件の賞賛

416件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please double check that you are not confused the MCU USB port cable and the BDM USB cable, MCU USB port has to be used in this case. 

Please connect already running board to USB port of the host.

Are you using a Freescale board?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛