The task period in the MQX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The task period in the MQX

841 Views
小勇邹
Contributor II

I create a 1ms period task in the MQX. I want to check whether the period is 1ms
at the beginning of the task. How can I measure the period by software method?

0 Kudos
3 Replies

411 Views
DavidS
NXP Employee
NXP Employee

Hi Robin,

Please look at this post:

elapsed time in nanoseconds

There is elapsed time in microseconds function call too.

Regards,

David

0 Kudos

411 Views
trailman
Contributor V

Hi,

You could use _time_get_ticks() to get two timestamps (one for previous run and one for current run) and use _time_diff_milliseconds() to return the difference in mS, or  _time_diff_microseconds() to get uS.

int ms;

boolean ms_overflow;

MQX_TICK_STRUCT ticks_last, ticks_cur;

_time_get_ticks(&ticks_last);

////

_time_get_ticks(&ticks_cur);

ms = _time_diff_milliseconds(&ticks_cur, &ticks_last, &ms_overflow);

For your 1mS task period, I remember that on MQX37 the system tick used for scheduling was set to 5mS by default (can be changed in BSP config), so a _time_delay(1); was sleeping for 5mS instead of 1mS. Take care of that with your task.

0 Kudos

411 Views
小勇邹
Contributor II

Thank you very much. I still have some questions.

1), If the system tick is set as 5ms, is it possible to call _time_diff_microseconds() to get uS?

2), After the task calls the function “_time_delay”,the task will
be blocked until the time is out.Is it right?

3), Is it possible to set the system tick as 1 us? If yes, how to set it?

4), What will happen if I set the task period as 1ms but I set
the time delay as 2ms in the task?

0 Kudos