I have some questions about the Freescale MQX RTC.
1,Does the Freescale MQX RTC have to work with MQX RTOS? Can it run in a simple main project?
2, The Freescale MQX RTCS is implemented as a C library. Do you provide the source code of the Freescale MQX RTCS?
3,How much memory does it cost when only DHCP and tftp applications are used?
已解决! 转到解答。
Hi Robin,
The RTCS is the TCPIP stack that must work together with the MQX RTOS. You cannot separate them. If you want a stand alone TCPIP stack then you may try
the FNET TCP/IP Stack.
The source code for the RTCS can be found in this path: C:\Freescale\Freescale_MQX_4_1\rtcs\source
We don't have the code size for the DHCP and tftp. However we have a tool that helps you to calculate this under the application that you are compiling. Take a look to this link to get more information on how to use it HOW TO GET THE CODE SIZE OF MQX4.1 PROJECT
Regards,
Garabo
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Robin,
The RTCS is the TCPIP stack that must work together with the MQX RTOS. You cannot separate them. If you want a stand alone TCPIP stack then you may try
the FNET TCP/IP Stack.
The source code for the RTCS can be found in this path: C:\Freescale\Freescale_MQX_4_1\rtcs\source
We don't have the code size for the DHCP and tftp. However we have a tool that helps you to calculate this under the application that you are compiling. Take a look to this link to get more information on how to use it HOW TO GET THE CODE SIZE OF MQX4.1 PROJECT
Regards,
Garabo
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Robin,
No, it can't. But you could use another processor expert component that includes a TCPIP RTOS. Take look to this link: FreeRTOS V8.0.0 Final Release available as Processor Expert Component | MCU on Eclipse
Hope it helps,
Regards,
Garabo