SPC5644A about etpu capture funtion driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5644A about etpu capture funtion driver

716 Views
happylu123
Contributor I

Hi ,

 

I'm a newer to the MPC5644A chips . I used eTPU module as input capture function to measure speed signal . I learn  AN2851SW  example1.c ,but the function does not work. the drive  as follows:

   


     SIU.PCR[191].R = 0x1100;        /* Initialize pad for eTPU_A[27]   input */
   


   fs_gpio_config ( FS_GPIO_ETPUA27, FS_GPIO_PRIMARY_FUNCTION + ETPU_INPUT_PAD_CONFIG);
    fs_etpu_init( my_etpu_config, (uint32_t *)etpu_code, sizeof(etpu_code),
                  (uint32_t *)etpu_globals, sizeof(etpu_globals));
    /* enable all timebases */
    fs_timer_start();
    SIU.ISEL8.B.ESEL3=1;           
 
     /* run eTPU IC function */
    error_code = fs_etpu_ic_init(IC_1, FS_ETPU_PRIORITY_MIDDLE, ETPU_IC_MODE_SINGLE,
         FS_ETPU_TCR1, ETPU_IC_RISING_EDGE, 1);
    
    while (ETPU.CISR_A.B.CIS27 != 1){}   //Wait for IC_1 (eTPU CH0 to complete)
    
    final_time = fs_etpu_ic_read_final_time (IC_1);  //Read value when last IC occurred
     
    while(1)
    {                                                     
     
     if(SysClk_ctPIT == 1000) 
     {          
        SysClk_ctPIT = 0;  //定时计数清零  
        
        final_time = fs_etpu_ic_read_final_time (IC_1);  //Read value when last IC occurred
       timelen=final_time ;
       CANA_TxData[0] = (uint8_t)((timelen&0xFF000000)>>24);
       CANA_TxData[1] = (uint8_t)((timelen&0x00FF0000)>>16);
       CANA_TxData[2] = (uint8_t)((timelen&0x0000FF00)>>8);
       CANA_TxData[3] = (uint8_t)(timelen&0x000000FF); 
       CANA_TxMsg();
     
        
        }
       

}

It stop at   while (ETPU.CISR_A.B.CIS27 != 1){} . finnal_time is always 0x0055C90B .

 

How to configure eTPU to realize capture function.

 

 

Best regards,

Labels (1)
0 Kudos
1 Reply

496 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I am not very familiar with eTPU, but here is working example for input capture.

regards,

Peter

0 Kudos