Hello,
well, there are some known issues listed in Release notes and it's planned to introduce a thread on this forum related to issues/workarounds. For now, please take a look here for the QSPI CS issue:
https://community.freescale.com/thread/63312
Sorry for confusion on sdcard initialization.
_io_sdcard_spi_init() function takes pointer to opened SDCARD file descriptor.
So in your case:
PetrM
Hi EDesign,
Currently the only SD Card example is with our twrmcf52259 Tower setup that has an additional Tower Memory card added that has the SD Card slot.
The m52259evb does not have SD Card slot but does have Compact Flash interface. That is supported via the PCFlash settings.
Regards,
David
Thank you David for the reply.
For anybody that has been able to get the SD card to work using QSPI, could you post example code for initialization? I am able to put the SD card into its "idle mode" state, but when I send commands "55" and "41", it is returning the wrong responses. I've successfully initialized an SD card before on a different microcontroller, but I'm not sure what I am doing wrong with the M52259EVB.
Hello,
there's an issue regarding QSPI CS assertion - when you try to access multiple SPI devices at the same time. The workaround is to use manual GPIO CS callbacks.
The other thing is correct setting of SPI and the initialization procedure itself - please refer to sdcard_spi.c, everything is there.
PetrM
PetrM,
I've been trying to get the sdcard_spi.c code to work with my eval board the past 2 days with no luck. For the following initialization function:
_io_sdcard_spi_init (MQX_FILE_PTR fd_ptr)
What exactly is fd_ptr refering to? Initially I thought it points to the QSPI, but MQX crashes at runtime with that.
Hello,
well, there are some known issues listed in Release notes and it's planned to introduce a thread on this forum related to issues/workarounds. For now, please take a look here for the QSPI CS issue:
https://community.freescale.com/thread/63312
Sorry for confusion on sdcard initialization.
_io_sdcard_spi_init() function takes pointer to opened SDCARD file descriptor.
So in your case:
PetrM