Rebuilding MQX doesn't update lib folder content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Rebuilding MQX doesn't update lib folder content

3,457件の閲覧回数
statrix
Contributor II

Hello All,

 

I need to rebuild MQX libraries because i want to enable ADC in my mcf52233DEMO board project, so i change this line at

user_config.h located at [installation]\config\[board]

 

#define BSPCFG_ENABLE_ADC        1    // ( 0 by default )

 

Then i follow the steps cited at the "FSL_MQX_Getting_Started.pdf" Rev 02 , section 2.4 ( CW 10.0). 

 

after rebuilding, for debug and release, if i go to the user_config.h file located under the \lib  directory it has the default line...so it's not being updated. 

I did a dedicated workspace for rebuilding MQX also.

 

I've tryed several things (building all at once, building one by one, in order, etc) but nothing changed the outcome. There are several warnings about not changing the user_config.h file under lib folder because it's replaced in each build. 

 

The only files being updated are bsp_m52233demo_d.a, bsp_m52233demo.a  

psp_m52233demo_d.a, psp_m52233demo.a  

 

Also, there is no mass build for this board for CW10, why ?.

 

I would be really thankful if someone can help me.

 

 

 

 

 

 

 

 

タグ(1)
0 件の賞賛
返信
5 返答(返信)

2,792件の閲覧回数
JuroV
NXP Employee
NXP Employee

What IDE do you use? CW7.2 or CW10?

0 件の賞賛
返信

2,792件の閲覧回数
statrix
Contributor II

Hello JuroV

 

Thanks in advance for helping me. There're a couple of mentions to CW10.0 in my post.  I apologize for not making

a explicit mention to it. That's the IDE i'm using (last build), under windows XP SP3.

 

Just let me know if you want me to try something.

0 件の賞賛
返信

2,792件の閲覧回数
statrix
Contributor II

So i guess it's only me the one who can't rebuild MQX.. what a loser! :smileysad:

 

Am i making some noob mistake that everyone sees?

 

Thanks in advance

0 件の賞賛
返信

2,792件の閲覧回数
JuroV
NXP Employee
NXP Employee

There's report that CW10 in some cases creates its own copies of sources and that's why you change user_config.h, but effectivelly you change only some copy of user_config.h. Personally I think it's better to refer this question to CodeWarrior team.

0 件の賞賛
返信

2,792件の閲覧回数
statrix
Contributor II

Thanks Jurov ! I'll do it and post here the solution.

 

 

0 件の賞賛
返信