I need to have a direct interrupt, which means MQX RTOS must not drive this interrupt. These interrupts come from Input Capture on all DMA and GPT pins. I managed to solve the problem using codewarrior 7.1 and MQX 3.3 and the following code. Unfortunately this is not working on Codewarrior 7.2 and MQX 3.61. What could I be missing? or what changes on MQX and compiler might affect the behavior of a working code?
extern void main_task(uint_32);const TASK_TEMPLATE_STRUCT MQX_template_list[] = { /* Task Index, Function, Stack, Priority, Name, Attributes, Param, Time Slice */ { MAIN_TASK, main_task, 1500, 5, "main", MQX_AUTO_START_TASK, 0, 0 }, { 0 }};__declspec(interrupt:0) void DMA_T3_ISR(pointer dummy_param){ VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR; reg_ptr->DMA_TIMER[ 3 ].DTER = 0b00000011; //Apaga las Banderas de Interrupcion}__declspec(interrupt:0) void DMA_T2_ISR(pointer dummy_param){ VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR; reg_ptr->DMA_TIMER[ 2 ].DTER = 0b00000011; //Apaga las Banderas de Interrupcion}/*Prueba para lector y tarjeta juntos*/__declspec(interrupt:0) void DMA_T1_ISR(pointer dummy_param){ VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR; reg_ptr->DMA_TIMER[ 1 ].DTER = 0b00000011; //Apaga las Banderas de Interrupcion}__declspec(interrupt:0) void DMA_T0_ISR(pointer dummy_param){ VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR; reg_ptr->DMA_TIMER[ 0 ].DTER = 0b00000011; //Apaga las Banderas de Interrupcion}void main_task ( uint_32 initial_data ){VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR; reg_ptr->GPIO.PORTTC = 0x00; /*GPIO Configuration for DMA Edge Triggered Interrupt 0 = Output low level*/ reg_ptr->GPIO.DDRTC = 0x00; /*GPIO Configuration for DMA Edge Triggered Interrupt 0 = Direction Input*/ reg_ptr->GPIO.PORTTCP_SETTC = 0x00; /*GPIO Configuration for DMA Edge Triggered Interrupt Nothing since it is input*/ reg_ptr->GPIO.CLRTC = 0x00; /*GPIO Configuration for DMA Edge Triggered Interrupt Nothing since it is input*/ reg_ptr->GPIO.PTCPAR = 0x55; /*GPIO Configuration for DMA Edge Triggered Interrupt Primary Function for all DTIM pins*/ reg_ptr->ICTRL0.ICR[19] = 0b01110011; //DES DMA_Timer[0] set to IL=7, IP=3 reg_ptr->ICTRL0.ICR[20] = 0b01110010; //DES DMA_Timer[1] set to IL=7, IP=2 reg_ptr->ICTRL0.ICR[21] = 0b01110001; //DES DMA_Timer[2] set to IL=7, IP=1 reg_ptr->ICTRL0.ICR[22] = 0b01110000; //DES DMA_Timer[3] set to IL=7, IP=0 reg_ptr->DMA_TIMER[ 0 ].DTMR = 0b0000000010000011; reg_ptr->DMA_TIMER[ 1 ].DTMR = 0b0000000010000011; reg_ptr->DMA_TIMER[ 2 ].DTMR = 0b0000000010000011; reg_ptr->DMA_TIMER[ 3 ].DTMR = 0b0000000010000011; reg_ptr->DMA_TIMER[ 0 ].DTXTMR = 0b01000000;//Everything Zero in order to: reg_ptr->DMA_TIMER[ 1 ].DTXTMR = 0b01000000;//1.- Have the timer increment by one reg_ptr->DMA_TIMER[ 2 ].DTXTMR = 0b01000000;//2.- Interrupt Enabled and DMA request disabled reg_ptr->DMA_TIMER[ 3 ].DTXTMR = 0b01000000;//3.- Timer Continues if core halts ( Dont need this feature , just trying to see if it works like this) reg_ptr->DMA_TIMER[ 0 ].DTER = 0b00000011; //Clear event condition reg_ptr->DMA_TIMER[ 1 ].DTER = 0b00000011; //Clear event condition reg_ptr->DMA_TIMER[ 2 ].DTER = 0b00000011; //Clear event condition reg_ptr->DMA_TIMER[ 3 ].DTER = 0b00000011; //Clear event condition reg_ptr->DMA_TIMER[ 0 ].DTCN = 0x0000; reg_ptr->DMA_TIMER[ 1 ].DTCN = 0x0000; reg_ptr->DMA_TIMER[ 2 ].DTCN = 0x0000; reg_ptr->DMA_TIMER[ 3 ].DTCN = 0x0000; *(unsigned int *) 0x2000014C = (unsigned int)&DMA_T0_ISR; //Install direct ISR vector for DTIM3 *(unsigned int *) 0x20000150 = (unsigned int)&DMA_T1_ISR; //Install direct ISR vector for DTIM3 *(unsigned int *) 0x20000154 = (unsigned int)&DMA_T2_ISR; //Install direct ISR vector for DTIM3 *(unsigned int *) 0x20000158 = (unsigned int)&DMA_T3_ISR; //Install direct ISR vector for DTIM3 _interrupt_controller_unmask(MCF5225_INT_DTIM0); //DES unmask DTIM3 _interrupt_controller_unmask(MCF5225_INT_DTIM1); //DES unmask DTIM3 _interrupt_controller_unmask(MCF5225_INT_DTIM2); //DES unmask DTIM3 _interrupt_controller_unmask(MCF5225_INT_DTIM3); //DES unmask DTIM3 while(1) { _time_delay(200); }}
The project builds and programs correctly but interrupts are never called.
I checked the thread you mention but I know the registers are correctly configured so that is not part of the problem.
I had MQX_ROM_VECTORS = 0 but then I changed it to 1 and the problem continues.