I meet a problem.I use K65 with MQX and RTCS.I need support VLAN Tag to connect switch.
I do this:
#define RTCSCFG_ENABLE_8021Q 1
but it doesn't work.Computer can ping K65,but can't open the web page on K65.
If something wrong i did?
Hi,
Please check the below link and let me know if this helps:
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
This link says that "#define RTCSCFG_LINKOPT_8021Q_PRIO 1" ,but i use MQX 4.4.0 witch have no "RTCSCFG_LINKOPT_8021Q_PRIO",but only " RTCSCFG_ENABLE_8021Q".
Yes, in MQX 4.2 it is RTCSCFG_ENABLE_8021Q. By default, RTCS does not send and receive Ethernet 802.1Q tags, Set this value to 1 to have RTCS send and receive Ethernet 802.1q (VLAN) tags.
Please see the RTCS user guider for more details
Regards
Daniel