Question about the Serial download Mode for iMX-8M-Plus-EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question about the Serial download Mode for iMX-8M-Plus-EVK

2,026 次查看
Harold
Contributor I

Dear members

I have iMX-8M-Plus-EVK and trying to download L4.14.78_1.0.0_ga_images_MX8MMEVK.zip image via Type-C Port1 and then run it. The board is in serial download mode (BOOT switch : 0001) .
I installed the https://ftdichip.com/wp-content/uploads/2021/08/CDM212364_Setup.zip with reference to https://ftdichip.com/wp-content/uploads/2020/08/AN_396-FTDI-Drivers-Installation-Guide-for-Windows-1....
However, when I turn on the Power Switch, Device Manager in Windows 10 catches the HID device on VID_1FC9 PID_0146.

 

D:\NXP>uuu L4.14.78_1.0.0_ga_images_MX8MMEVK.zip
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.149-0-gab2f4c7

Success 0 Failure 0 Wait for Known USB Device Appear...

Prep 1/ 0 [=================100%=================] Http Download\Uncompress

D:\NXP>uuu L4.14.78_1.0.0_ga_images_MX8MMEVK.zip
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.149-0-gab2f4c7

Success 0 Failure 1

Prep 1/ 0 [======> 19% ] Http Download\Uncompress
1:2 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk

Linux is also recognized as VID_1FC9 PID_0146 and is not recognized as Virtual Serial Port.
pi@raspberrypi:~ $ lsusb
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 001 Device 004: ID 046d:c534 Logitech, Inc. Unifying Receiver
Bus 001 Device 005: ID 1fc9:0146 NXP Semiconductors
Bus 001 Device 002: ID 2109:3431 VIA Labs, Inc. Hub
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

What's the problem?

0 项奖励
回复
2 回复数

588 次查看
Chethan_TS
Contributor I

Hi, 

 

I am facing similar issue when trying to download image via C-type port1 to my iMX-8M-PLUS-Evaluation kit

-i tried with both the images L4.14.78_1.0.0_ga_images_MX8MMEVK.zip and LF_v6.1.55-2.2.0_images_IMX8MMEVK.zip where the latter being the latest image .

Chethan22_1-1711007349390.png

 

i don't understand the problem.

 

PS : i have installed the required USB drivers and the Boot switch is set to 0001 i.e Serial download 

0 项奖励
回复

1,945 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

I found that you are using the iMX-8M-Plus-EVK board but you are using the  images L4.14.78_1.0.0_ga_images_MX8MMEVK.zip for i.MX8MM EVK board, so failure you can see 1:2 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk

And the Linux 4.14.78_1.0.0 is not the GA release BSP for the i.MX8MP EVK board, you can select the right demo images here:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

0 项奖励
回复