I did not try TWR-WIFI-AR4100 but could you please try the latest MQX v4.0.1 which is available at:
http://www.freescale.com/webapp/sps/site/overview.jsp?code=MQXSWDW
I see that there is an enablement patch for 3.8 that was recently released.
Has anyone been successful in integrating this into MQX 3.8 and getting this to work?
I have successfully got the TWR-AR4100 working with MQX 3.7 on the TWR-K60n512. But am not able to get MQX 3.8 with the new 3.8 patch working.
I am using a 4100 not a 4100P.
Just wanted to know if anyone has got this working before I go any further.
thanks
Doug
Hi ,
Check this : https://community.freescale.com/thread/304770
May be helpful.Also you need to keep TCP/IP stack option too
as you are using AR4100. Also complete documentation given
with Atheros driver , you can follow the step.
Also check the SPI driver.It may have some difference. At present I am trying
with TWR-K60F120M , but still no luck with MQX73.7 (AR4100 patch) with MQX4.0.
Hi,
I installed the MQX 3.6.2 and the TWR-WIFI-AR4100 MQX 3.6.2 Enablement Patch (Rev1.5) which
were downloaded from the freescale.com/TowerWiFi. But I could not build the bsp target.
The error messages told below
"Could not find or load the file a_config.h for target RegABI for project bsp_trrmcf5229_ATHROS_WIFI.mcp0"
"Could not find or load the file a_debug.h for target RegABI for project bsp_trrmcf5229_ATHROS_WIFI.mcp0"
"Could not find or load the file a_drv.h for target RegABI for project bsp_trrmcf5229_ATHROS_WIFI.mcp0"
"Could not find or load the file a_drv_api.h for target RegABI for project bsp_trrmcf5229_ATHROS_WIFI.mcp0"
"Could not find or load the file a_osapi.h for target RegABI for project bsp_trrmcf5229_ATHROS_WIFI.mcp0"
"Could not find or load the file a_debug.h for target RegABI for project bsp_trrmcf5229_ATHROS_WIFI.mcp0"
"Could not find or load the file a_drv.h for target RegABI for project bsp_trrmcf5229_ATHROS_WIFI.mcp0"
"Could not find or load the file a_drv_api.h for target RegABI for project bsp_trrmcf5229_ATHROS_WIFI.mcp0"
"Could not find or load the file a_osapi.h for target RegABI for project bsp_trrmcf5229_ATHROS_WIFI.mcp0"
and so on.
And the MQX 3.6.2 Enablement Patch did not install these files( a_config.h, a_debug.h, a_drv.h ... ).
Would you give me any advice.
Thanks
Shoji
Hi,
I try to use the TRW-WIFI-AR4100 module, but I cannot setup QMX with the patch.
I am using IAR compiler so I tried to setup QMX 3.6.2 and the driver patch but when I try to rebuild the project, I have mssing files. All files in the project under mqx/source/io/enet/atheros_wifi are missing.
I installed QMX 3.6.2 and after this I installed the TWR-WIFI-AR4100 MQX 3.6.2 Enablement Patch.
Has anybody already been able to run 1 demo of the wifi modules?
Thanks
I have not tried others but Redpine module along with patch for mqx 3.7 works fine... but u will have to do some changes in the process.. forum https://community.freescale.com/message/106090#106090 and https://community.freescale.com/message/106036#106036 will help u in this regard..
Kind regards,
Abhinav
Hi,
I'm tying to testing the TWR-WIFI-AR4100 board with a MCF52259 (TWR board too).
But I'm not able to have the demo and config directories for my target, only for Kinetis...
There is a PDF file which describes the installation :
http://cache.freescale.com/files/wireless_comm/doc/support_info/TWRWIFIAR4100LAB.pdf
But the MQX version is 3.6. I can not start a new project with an older version of the OS !
My computer OS is Win XP, and I tried on my laptop under Win 7 ; the same.
Any ideas ? This board seems not to be used a lot in the world :smileysad:
Regards,
Yvan