I have K70 system running MQX4.0 with both an USB and SD card interface. When using the shell (Shell_Copy) to copy files from the USB card to the SD card, they become corrupt. Copying from SD to USB is not a problem. Attachment is sample corrupt file. The only thing I tried was to increase the shell task's stack size (from 12,000 to 50,000).
We wrote our own copy routine that:
1. Opens (fopen) a 'from' and 'to' file
2. using freads() and fwrites(), copies one file to the other
3. Closes (fclose) both files
Like 'Shell_copy' the hand written copy routine does not function when copying from a USB card to an SD card.
By printing out the 'copied' data we determined that it is the fread() that fails (i.e. it just returns bad data).
More investigation showed that the first fread() always returns good data but each subsequent ones return bad data.
Hi
From your description, it seems a MFS issue. I suggest you upgrade to MQX 4.2.0, patched with the latest patch 4.2.0.2. We made some improvements in MFS in this version. I think it may solved your issues.
Regards
Daniel
It is a custom board. MQX can write to the SD card...it's the data that is corrupt. Not all the file just parts of it. Open the attachment and you can see that the copied file is mostly correct.