Hello, I am trying to install S32 Design Studio for vision in Linux and facing the following error: Extracting the installation resources from the installer archive... Configuring the installer for this system's environment... No Java virtual machine could be found from your PATH environment variable. You must install a VM prior to running this program.
The command i have used to install S32 Design Studio for vision in Linux is given below:
ll_stmdanay@livinglab-CELSIUS-W550power:~$ nano ~/.bashrc
The below two lines i have added in .bashrc to define the path of java:
export PATH=/usr/local/jdk-11/bin:$PATH
export JAVADIR=/usr/local/jdk-11/
ll_stmdanay@livinglab-CELSIUS-W550power:~$ source ~/.bashrc
ll_stmdanay@livinglab-CELSIUS-W550power:~$ cd Downloads
ll_stmdanay@livinglab-CELSIUS-W550power:~/Downloads$ sudo chmod +x ./S32DS_Vision_Linux_v2018.R1_b181126.bin
[sudo] password for ll_stmdanay: ******
ll_stmdanay@livinglab-CELSIUS-W550power:~/Downloads$ sudo ./S32DS_Vision_Linux_v2018.R1_b181126.bin
It will be great help if someone help me to solve this problem.
Best Regards
Anayat
Hello Jiri,
My java-version command is:
ll_stmdanay@livinglab-CELSIUS-W550power:~$ java -version
openjdk version "10.0.2" 2018-07-17
OpenJDK Runtime Environment (build 10.0.2+13-Ubuntu-1ubuntu0.18.04.4)
OpenJDK 64-Bit Server VM (build 10.0.2+13-Ubuntu-1ubuntu0.18.04.4, mixed mode)
ll_stmdanay@livinglab-CELSIUS-W550power:~$ whereis java
java: /usr/bin/java /usr/share/java /usr/share/man/man1/java.1.gz
ll_stmdanay@livinglab-CELSIUS-W550power:~$ which java
/usr/bin/java
Hello Jiri,
I am using Ubuntu and tried installing 11.0.4 and then 11.0.3.
bob@Ubuntu:/etc/devkit$ java -version
java version "11.0.3" 2019-04-16 LTS
Java(TM) SE Runtime Environment 18.9 (build 11.0.3+12-LTS)
Java HotSpot(TM) 64-Bit Server VM 18.9 (build 11.0.3+12-LTS, mixed mode)
I tried your suggestion:
sudo apt-get install openjdk-8-jre
Java installed, but S32 still does not install. Do I need to remove all of the Java installations and then install version 8?
Thanks,
Bob