Yes, this is another PWM driver for MCF5225x, but when I wrote it no driver was available.
Snce this time a driver was posted on the forum by Myke (https://community.freescale.com/message/69804#69804)
I post mine now in cas it would help.
It only has 3 IOCTLs :
- one to init PWM module
- one to init a pin for PWM and set an initial period and duty
- one to update period/duty.
It has been written to drive some fans.
To use it :
- in mqx/source/include/ioctl.h , add the following #define
#define IO_TYPE_GPTIN 0xNN
where 0xNN is an unused value for your BSP
- in mqx/source/psp/coldfire/mcf5225.h , in mcf5225_pwm_struct, replace :
uchar filler[0xFFDB];
with
uchar filler3;
uchar PCME; // PWM PCM Mode Enable register
uchar filler[0xFFD9];
- install the driver source files in mqx/source/io
- then use the driver using its simple API :
Install driver :
_io_pwm_install("pwm:");
Open device ;
FILE_PTR fdpwm;
if ((fdpwm = fopen("pwm:", NULL )) == NULL) {
printf("Opening PWM device driver failed.\n");
}
Configure PWM module :
PWM_DEV_CONFIG_DATA pwm_conf_data;
pwm_conf_data.clock_Sys_to_A_divisor = 0; /* 2**n, 0<=n<=7 */
pwm_conf_data.clock_Sys_to_B_divisor = 0; /* 2**n, 0<=n<=7 */
pwm_conf_data.clock_A_to_AS_divisor = 60; /* 2*n, or 512 if n=0 */
pwm_conf_data.clock_B_to_BS_divisor = 60; /* 2*n, or 512 if n=0 */
if (ioctl(fdpwm, PWM_IOCTL_CONFIG, &pwm_conf_data)) {
printf("PWM_IOCTL_CONFIG failed.\n");
}
Configure a pin and set initial period and duty cycle :
pwm_pin_data.pwm_pin = 2; /* 0-7 */
pwm_pin_data.polarity = 1; /* 1 for active high */
pwm_pin_data.xS_clock_select = 1; /* 1 for AS/BS clock instead of A/B; A for 0,1,4,5 / B for 2,3,6,7 */
pwm_pin_data.center_aligned = 0; /* 1 for center aligned */
pwm_pin_data.concatenate = 0; /* 1 to concatenate odd channel n with channel n-1 */
pwm_pin_data.stop_doze = 0; /* stop PWM in doze mode */
pwm_pin_data.stop_debug = 0; /* stop PWM in debug mode */
pwm_pin_data.pcm_enable = 0; /* 1 to use PCM instead of PWM */
pwm_pin_data.period = 200; /* 0-255, or 0-65535 if concatenate=1 */
pwm_pin_data.duty = 0; /* 0-period; 0:0%; period:100% */
if (ioctl(fdpwm, PWM_IOCTL_ENABLE_PIN, &pwm_pin_data)) {
printf("PWM_IOCTL_ENABLE_PIN failed.\n");
}
Change period and duty cycle :
pwm_change_data.pwm_pin = 2;
pwm_change_data.period = 200;
pwm_change_data.duty = 70; /* 35 % PWM (70 for 200) */
if (ioctl(fdpwm, PWM_IOCTL_CHANGE_DUTY, &pwm_change_data)) {
printf("PWM_DEV_CHANGE_DUTY_DATA failed.\n");
_mqx_exit(-1);
}
已解决! 转到解答。
I found an error in my first post : you must edit mqx/source/include/ioctl.h to add :
#define IO_TYPE_PWM 0xNN
where 0xNN is an unused value for your BSP
not IO_TYPE_GPTIN (this was a copy of another post for a GPTIN driver)