Hi all,
I need to configure my UART(2) to use RTS flow control on the MCF52259. I can use the UART normally with IO_SERIAL_RAW_IO no problem, but cant get RTS working. I checked PUCPAR and it is set to one indicating primary function of RTS on pin 82 (PUC3).
I tried many experiments, settings, configurations yesterday and this morning. I have posted some simple test code below that hopefully someone can look at and quickly tell me what I have done wrong, or why its not working. I have no experience with hardware flow control really, Ive used it on other projects and it "just worked" so I didnt have to look into it.
//Auto start task
void SDI_Task(void)
{
uint_32 temp = 0;
pointer Comm3_IO;
uint_8 SDI_TX_BUFF[512] = {0};
//Needs to have 9 bit data, always set low, so I tried this >>
Comm3_IO = (pointer)fopen("ittyc:", (pointer)(IO_SERIAL_RAW_IO));
//PUCPAR bit 3 becomes set ifi printf PUCPAR or stop debugger and check it...
//9 bit data always low for this application
temp = IO_SERIAL_PARITY_SPACE;
ioctl(Comm3_IO, IO_IOCTL_SERIAL_SET_PARITY, &temp);
//For a simple test to see if I could just get RTS to change state I tried this >> (this does nothing)
temp = IO_SERIAL_RTS;
(void)ioctl(Comm3_IO, IO_IOCTL_SERIAL_SET_HW_SIGNAL, &temp);
_time_delay(100);
(void)ioctl(Comm3_IO, IO_IOCTL_SERIAL_CLEAR_HW_SIGNAL, &temp);
_time_delay(100);
(void)ioctl(Comm3_IO, IO_IOCTL_SERIAL_SET_HW_SIGNAL, &temp);
_time_delay(100);
(void)ioctl(Comm3_IO, IO_IOCTL_SERIAL_CLEAR_HW_SIGNAL, &temp);
_time_delay(100);
(void)ioctl(Comm3_IO, IO_IOCTL_SERIAL_SET_HW_SIGNAL, &temp);
sprintf(SDI_TX_BUFF, "123456789");
for(;;)
{
_time_delay(1000);
//CTS is manually tied high with a 10K resistor, tried high and low with no change
//I tried first setting and/or clearing the RTS as above, but still nothing
fprintf(Comm3_IO, "%s", SDI_TX_BUFF);
}
}
To start testing i quickly wrote some code which works for a simple test to emulate what I need from RTS.
If MQX's RTS control on ittyc / ttyc is an issue, maybe someone could indicate where in the MQX source I can add two lines marked "//RTS high" and "//RTS low" as this would be fine for my application?
This code works fine for testing, but, I must meet a protocol specification that requires RTS low to happen within 25uS of the final stop bit, and I simply cannot stop my processor like I am below in a loop waiting for the TEMP flag in USR to clear, it would have to be interrupt driven in some way, or, maybe someone has some other ideas?
Comm3_IO = (pointer)fopen("ittyc:", (pointer)(IO_SERIAL_RAW_IO | IO_SERIAL_PARITY_SPACE | IO_SERIAL_STOP_BITS_1));
reg_ptr->GPIO.PUCPAR &= (~0b00000100); //Force to GPIO
reg_ptr->GPIO.DDRUC |= 0b00000100; //Force to output state
reg_ptr->GPIO.PORTUC &= (~0b00000100); //Force to output to low
sprintf(SDI_TX_BUFF, "123456789");
for(;;){
_time_delay(1000);
reg_ptr->GPIO.PORTUC |= 0b00000100; //RTS high
fprintf(Comm3_IO, "%s", SDI_TX_BUFF);
fflush(Comm3_IO);
while((reg_ptr->UART[2].READ.USR & 0x08) == 0);
reg_ptr->GPIO.PORTUC &= (~0b00000100); //RTS low
}
Hi Carl:
I think you can try the io open flag "IO_SERIAL_HW_FLOW_CONTROL"
For see the MQX_IO_User_Guide.pdf for more details
it is located on your installation folder
C:\Freescale\Freescale_MQX_4_2\doc\mqx
Here is an example:
void Main_task(uint_32 initial_data)
{
uint_32 flags=IO_SERIAL_HW_FLOW_CONTROL;
MQX_FILE_PTR pfile1;
MQX_FILE_PTR pfile2;
pfile1 = fopen("ittyc:", NULL);
pfile2 = fopen("ittya:", NULL);
ioctl(pfile1,IO_IOCTL_SERIAL_SET_FLAGS, &flags);
ioctl(pfile2,IO_IOCTL_SERIAL_SET_FLAGS, &flags);
printf("\n Hello World \n");
_time_delay(240000);
fclose(pfile1);
fclose(pfile2);
_mqx_exit(0);
}
Regards
Daniel
Thank you Daniel,
I made the following changes to my example based on your example
1. fopen pass NULL
2. Separate call to IO_SERIAL_HW_FLOW_CONTROL using IO_IOCTL_SERIAL_SET_FLAGS
3. changed your printf("\n Hello World \n"); to fprintf(Comm3_IO, "%s", &SDI_TX_BUFF[0]);
Unfortunately no luck. RTS always high. If I call fflush(Comm3_IO); it never returns...
From what you have posted, really you have just pointed out not to pass flags in the fopen call which i thought was ok? I get the same result if I pass flags with fopen or set it after... I did this because MQX example pass flags with fopen. MQX's on examples do this, this is copy and pasted from the example supplied by MQX
rs485_dev = fopen( RS485_CHANNEL, (char const *)IO_SERIAL_HW_485_FLOW_CONTROL );