Hi,I am a rookie. I have downloaded MQX4.0 in my PC which installed XP System and used IAR 6.2 to build the MQX web_hvac demo.
I didn't modify anything of the codes and have not connected the hardware. I just built the IAR workspace in MQX4.0, which is located
at the folder <installed MQX path>/config/twrk60n512\iar\build_libs.eww. And there has been the .a files which I need in the web_hvac example.
But here comes the problem as following:
Linking
Error[Li005]: no definition for "__DEFAULT_PROCESSOR_NUMBER" [referenced from mqx_init.o(bsp_twrk60n512_d.a)]
Error[Li005]: no definition for "__KERNEL_DATA_END" [referenced from mqx_init.o(bsp_twrk60n512_d.a)]
Error[Li005]: no definition for "__DEFAULT_INTERRUPT_STACK_SIZE" [referenced from mqx_init.o(bsp_twrk60n512_d.a)]
Error[Li005]: no definition for "__VECTOR_TABLE_ROM_START" [referenced from init_bsp.o(bsp_twrk60n512_d.a)]
Error[Li005]: no definition for "__EXTERNAL_MRAM_RAM_BASE" [referenced from init_hw.o(bsp_twrk60n512_d.a)]
Error[Li005]: no definition for "__BOOT_STACK_ADDRESS" [referenced from vectors.o(bsp_twrk60n512_d.a)]
Error while running Linker
Could anyone help me!
Thanks a million!
Ming
解決済! 解決策の投稿を見る。
I'm afraid about the IAR version 6.2. MQX 4.0 release was compiled and tested with IAR 6.4 (and I know it works also with IAR 6.5). Based on the errors you list it seems that 6.2 has problems to read 6.4 linker command file.
Hello
I have this same linker error in IAR 6.30. As Mr. Martin mentioned, I rebuilt all my libraries with IAR 6.60.1 Evaluation version and tried to rebuild helloworld MQX example
for twrK60DN512. But the Linker error is still there.
Please tell me where I am mistaking. If you had solved this problem, Please give step by step instructions to overcome this.
many Thanks in advance
I'm afraid about the IAR version 6.2. MQX 4.0 release was compiled and tested with IAR 6.4 (and I know it works also with IAR 6.5). Based on the errors you list it seems that 6.2 has problems to read 6.4 linker command file.