I am using MQX™ RTOS 3.7.0. But repeated attempt to write on SD card (of 2GB) constantly failing at about 900MB. I am using different file sizes. And this failure is not related to number of file is written as I have already tried write 160 to 500 files with different sizes. But in all cases it fails exactly around 900MB.
Pseudo code:
fopen_s(&FileHandle, file_name_and_path, "w");
if( pFileHandle ) {
Div_Count = Buff_len / 255;
while( Div_Count-- ) {
fprintf(pFileHandle, Sample_Buff_with_255char);
}
fclose(pFileHandle);
OS_Sleep(1000);
When I am trying t read the file, the read buffer does not match with written data. This failure happens only after 900MB of write.
Hi Nilay:
From your description, it seems a MFS issue. I believe this issue is fixed in the latest MQX version.
MQX 3.7 is a very old version. I would suggest you update to MQX 4.2.0, and with patch MQX 4.2.0.2 , MFS FAT file system is more stable than that in MQX 3.7.
Regards
Daniel