MQX SPI Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX SPI Driver

665件の閲覧回数
louiemoye
Contributor III

Hello - does anyone have experience using the MQX SPI driver where Chip Select toggling is required?  I'm just wondering how this is accomplished (if possible) maybe using ioctl?  I need to have the ability to switch between toggling and not, as I have two devices on the bus - one requires toggle and the other not.  I'm able to do it with PE (SPI2_SelectConfiguration), but I need to use only MQX SPI driver. 

Using K70 with CW10.6, MQX 4.1.

Best regards,

Louie

タグ(3)
0 件の賞賛
返信
2 返答(返信)

510件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Louie:

A single callback function for CS handling may be registered per SPI device. The callback function registration is performed by the IO_IOCTL_SPI_SET_CS_CALLBACK_IOCTL command. The parameter of the command is SPI_CS_CALLBACK_STRUCT which contains a pointer to the callback function and a pointer to the arbitrary context data for the callback function.

SPI driver then calls the function any time when a change of the CS signals state is necessary. Besides the context data, the function is also passed a desired state of the CS signals. The callback function is then responsible for changing the state of the CS by any method (e.g., using LWGPIO)


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct or helpful button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

510件の閲覧回数
louiemoye
Contributor III

Thanks, Daniel.  I have started down the path of registering the callback. I wasn't sure if there was a way to have hardware do the toggling/strobing since the SPI port can be configured to handle the /CS line, but apparently it's required in software.  I will look into controlling the /CS line manually.

0 件の賞賛
返信