MQX Enable Low Power flag

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX Enable Low Power flag

472 Views
noamziv
Contributor I

Question:

When using KDS3.0, KSDK1.3 and MQXLite - how do I configure the project to set the MQX_ENABLE_LOW_POWER flag and remove the idle loop counter?

Details:

I am in the process of converting (read - re writing) a project.

The existing project uses KDS2.0 and MQXLite, but not KSDK.

The new project uses KDS3.0, KSDK1.3 and MQXLite.

Both projects create an Idle Task

The Idle Task makes use of two flags:

MQX_ENABLE_IDLE_LOOP  - Idle task implements a counter, preventing transitions to lower power states

MQX_ENABLE LOW_POWER - counter is replaced with _ASM_SLEEP

Also, when looking at the idle task file  (an idletask.c file is placed in the ../SDK/rtos/mqx/source/kernel directory),

another troubling fact is the following line (found prior to the code for the idle loop):

#if !defined(MQX_ENABLE_IDLE_LOOP) || MQX_ENABLE_IDLE_LOOP

counter code

#endif

which is pretty much the same as #if TRUE (i.e. always implement the counter)

Many thanks!

0 Kudos
Reply
0 Replies