MQX 3.8 GPIO on MCF52235 ( fopen("gpio:read",... ) problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX 3.8 GPIO on MCF52235 ( fopen("gpio:read",... ) problem

Jump to solution
1,229 Views
lupogrigio
Contributor III

Hi All,

 

I have a problem doing a very simple operation using the gpio driver, both as simple pin and as 

interrupt pin. I have controlled things as pin definition, irq capability...yet

 

I'm simply trying to read an input pin (a button in MCF52235EVB) by mean of the gpio driver, but the program

end after trying to open the input file descriptor, and say "Error opening pin file".

 

I have found a similar post of the past year reporting this error, but no solution is provided. I don't now if

it is an error due to porting from MQX 3.7 to MQX 3.8. The instruction I'm following to leanr MQX are based on

the 3.5 version.

 

The operation I do are: 

 

0. Define the pin

     #define SW1 (GPIO_PORT_NQ | GPIO_PIN4 | GPIO_PIN_IRQ) 

1. Define a file descriptor  

     static FILE_PTR input_file = NULL;

2. Define the pin list array

    uint_32 input_pins [] =  {SW1, GPIO_LIST_END };

3. Define the Task template and...

   TASK_TEMPLATE_STRUCT MQX_template_list[] = { 

       {MAIN_TASK, Main_task, 1500, 5, "main", MQX_AUTO_START_TASK}, 

       {0, 0, 0, 0, 0, 0, }
    };

4. Open the input file inside MainTask procedure

       void Main_task(uint_32 initial_data) {
       printf("\n GPIO Driver ---- Lab.2 ---- \n");
       input_file = fopen("gpio:input", (char_ptr) &input_pins);    
       if (input_file)        {
           printf("Pin file opened. \n");
        } else    {

          printf("Error opening pin file - Error n. %d. \n",input_file);
         _mqx_exit(0);      // <--------- PROGRAM END HERE!!!!
        }

      if (IO_OK != ioctl(input_file,GPIO_IOCTL_SET_IRQ_FUNCTION,(char_ptr) &PinISR)) {
         printf("Register IRQ failed. \n");
        _mqx_exit(-1);
     }

    while (TRUE) { // loop here  }
   // FOLLOW ISR DECLARATION ETC.. 

_mqx_exit(0);

}

 

 

Thanks in advance to anyone can solve this.

 

Giulio

 



 

 

0 Kudos
1 Solution
438 Views
lupogrigio
Contributor III

Solved!

 

The solutuin is to set:

 #define BSPCFG_ENABLE_GPIODEV    1

in user_config.h

 

Maybe this kind of settlement wasn't necessary in earlier versions, but it doen's matter....

 

Bye

 

 

 

View solution in original post

0 Kudos
4 Replies
438 Views
lupogrigio
Contributor III

Hi all,

 

at point 4 I have make a mistake copying the code, the open istruction is

   input_file = fopen("gpio:read", (char_ptr) &input_pins);

instead of

  input_file = fopen("gpio:input", (char_ptr) &input_pins);

 

The problem, obviusly, isn' solved, and is the same as reported on the preceding post.

 

G.

 

 

 

0 Kudos
439 Views
lupogrigio
Contributor III

Solved!

 

The solutuin is to set:

 #define BSPCFG_ENABLE_GPIODEV    1

in user_config.h

 

Maybe this kind of settlement wasn't necessary in earlier versions, but it doen's matter....

 

Bye

 

 

 

0 Kudos
438 Views
DavidS
NXP Employee
NXP Employee

Hi Giulio,

Congratulations on getting the GPIO to work.  That driver is big and abstracted greatly so you did good work.

As FYI the GPIO driver is being deprecated.  The LWGPIO driver is much more compact and efficient.  If you can switch I'd recommend doing so.

Regards,

David

0 Kudos
438 Views
Fabi
Contributor III

Similar topic, another question: Is it possible to have more than once callback functions to handle the GPIO interrupt?

Example:

GPIO_PIN_STRUCT gpio_1[] = {BSP_SW1|GPIO_PIN_IRQ_RISING, BSP_SW2|GPIO_PIN_IRQ_RISING, GPIO_LIST_END};
GPIO_PIN_STRUCT gpio_2[] = {BSP_SW3|GPIO_PIN_IRQ_RISING, BSP_SW4|GPIO_PIN_IRQ_RISING, GPIO_LIST_END};
hd1 = fopen ( "gpio:read", (char_ptr)&gpio_1 );

hd2 = fopen ( "gpio:read", (char_ptr)&gpio_2 );

ioctl ( hd1, GPIO_IOCTL_SET_IRQ_FUNCTION, (pointer)gpio_callback_1 );

ioctl ( hd2, GPIO_IOCTL_SET_IRQ_FUNCTION, (pointer)gpio_callback_2 );

0 Kudos