Hi,
my program works fine when I use "ttye:" as default console, but after I recompiled the psp and bsp to use "ittye:", there is no output on the default console.
please help with any clue. Thanks.
user_config.h
#define BSPCFG_ENABLE_TTYE 0
#define BSPCFG_ENABLE_ITTYE 1
twrk60n512.h
#if BSPCFG_ENABLE_ITTYE
#define BSP_DEFAULT_IO_CHANNEL "ittye:"
#define BSP_DEFAULT_IO_CHANNEL_DEFINED
#else
#define BSP_DEFAULT_IO_CHANNEL NULL
#endif
#ifndef BSP_DEFAULT_IO_OPEN_MODE
// #define BSP_DEFAULT_IO_OPEN_MODE (pointer) (IO_SERIAL_XON_XOFF | IO_SERIAL_TRANSLATION | IO_SERIAL_ECHO)
#define BSP_DEFAULT_IO_OPEN_MODE (pointer) (IO_SERIAL_RAW_IO /* | IO_SERIAL_NON_BLOCKING*/ )
#endif
my code
// read from ittyf and write to ittye(default console)
fd = fopen ("ittyf:", (pointer) (IO_SERIAL_RAW_IO));
for (;
{
i=fread(&data, 1, 1, fd);
if :smileyinfo: putchar(data);
}
已解决! 转到解答。
I had the similar problem. Try compiling psp and bsp both debug and release libraries. It should work.
Also UART4 that is TTYE had pinouts at a differnet port as given on schematics. Check out _bsp_serial_io_init function in init_gpio.c file . It should give you some clue where TTYE pinouts are connected.
I had the similar problem. Try compiling psp and bsp both debug and release libraries. It should work.
Also UART4 that is TTYE had pinouts at a differnet port as given on schematics. Check out _bsp_serial_io_init function in init_gpio.c file . It should give you some clue where TTYE pinouts are connected.