I try to include the TSS capabilities of the TWRK40X256 board (Touch Electrodes) into an application.
The TSS example compiles and works as intended.
When I use the same code from the example in my own application I get some weird errors in my BSP project about missing definitions. I can't figure out what I missed while porting the example. The references to /lib/twrk40x256.cw10/debug/bsb/tss exist.
I attached a screenshot with the code that causes the errors and the error list.
I use CodeWarrior 10.2 with MQX 4.0.
Thanks for any help
Solved! Go to Solution.
Hello Frieder Schrempf,
can you compare linker path settings with the original HMI application (in your monitor application). Are all paths same set ?
It would help you paste them here, linker settings in your application. BSP does not include TSS library, the application's linker must resolve all symbols.
Regards,
MartinK
Hello Frieder Schrempf,
can you compare linker path settings with the original HMI application (in your monitor application). Are all paths same set ?
It would help you paste them here, linker settings in your application. BSP does not include TSS library, the application's linker must resolve all symbols.
Regards,
MartinK
Thank you for the quick help!
I did not know that the library has to be added manually.
After including "tss.a" in the Linker settings everything worked.