Is there any chance / option to get FTP Server Events? Like File received complete ..

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any chance / option to get FTP Server Events? Like File received complete ..

Jump to solution
453 Views
monXii
Contributor III

Hello all,

 

i am using the MQX 3.8 .. and has running the FTP Server on my custom K60 board ..

all fine! :smileyhappy:

 

but now it would be nice to have an event for some actions ..

like file received compete ..

like user logged in ..

 

and so on :smileyhappy:

 

.. is there something in it? or i have to modify the rtcs ?

 

thanks so far!

Labels (1)
Tags (1)
0 Kudos
1 Solution
288 Views
monXii
Contributor III

it does not look like there is a rdy solution ..

 

.. i just have modified the ftpd_cmd.c for my callbacks .. :smileyhappy:

 

the fastest and easiest way :smileywink:

 

thanks so far! :smileyhappy:

View solution in original post

0 Kudos
1 Reply
289 Views
monXii
Contributor III

it does not look like there is a rdy solution ..

 

.. i just have modified the ftpd_cmd.c for my callbacks .. :smileyhappy:

 

the fastest and easiest way :smileywink:

 

thanks so far! :smileyhappy:

0 Kudos