I wanna design the MQX 3.8.1 (MK60FN1M0VLQ12) to configure the dual storage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I wanna design the MQX 3.8.1 (MK60FN1M0VLQ12) to configure the dual storage

432 次查看
stevejin
Contributor I

Hi.

I wanna design the MQX 3.8.1 (MK60FN1M0VLQ12) to configure the dual storage of the NAND flash on the board and an external SD card system.

I need Reference code.

PLS.

Can you tell me a Solution?

Design Environment

     MCU              : MK60FN1M0VLQ12 

     COMPILER   : IAR 6.7 / MQX TAD Plugin 4.6.6.0 

    OS                 : MQX 3.8.1

    JTAG             : PE micro Multilink

BR

Steve Jin

0 项奖励
1 回复

244 次查看
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately MQX 3.8 doesn't include support for NAND Flash driver for K60 devices, I suggest to migrate to the last MQX release.

For MQX 4.2, you can find the below examples, these examples may help

C:\Freescale\Freescale_MQX_4_2\mfs\examples\sdcard

C:\Freescale\Freescale_MQX_4_2\ffs\examples\mfs_nandflash

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励