Hi.
I wanna design the MQX 3.8.1 (MK60FN1M0VLQ12) to configure the dual storage of the NAND flash on the board and an external SD card system.
I need Reference code.
PLS.
Can you tell me a Solution?
Design Environment
MCU : MK60FN1M0VLQ12
COMPILER : IAR 6.7 / MQX TAD Plugin 4.6.6.0
OS : MQX 3.8.1
JTAG : PE micro Multilink
BR
Steve Jin
Hi,
Unfortunately MQX 3.8 doesn't include support for NAND Flash driver for K60 devices, I suggest to migrate to the last MQX release.
For MQX 4.2, you can find the below examples, these examples may help
C:\Freescale\Freescale_MQX_4_2\mfs\examples\sdcard
C:\Freescale\Freescale_MQX_4_2\ffs\examples\mfs_nandflash
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------