hello all,
I used KDS3.0 and based on MQX4.2 and KSDK1.2 project, my board is twrk64f120m,
the task scheduling to me have a little bit of problem
I have add the TCPIP tasks and it was worked ok before,
But when I add the CAN bus program to initialization,
it looks like that the task is blocked in lwsem.c as below
could you know what's the problem?
{
sem_chk_ptr = (LWSEM_STRUCT_PTR) ((void *) kernel_data->LWSEM.NEXT);
while (sem_chk_ptr != (LWSEM_STRUCT_PTR) ((void *) &kernel_data->LWSEM))
{
if (sem_chk_ptr == sem_ptr)
{
/* remove semaphore from kernel LWSEM queue */
_QUEUE_REMOVE(&kernel_data->LWSEM, sem_ptr);
break;
} /* Endif */
sem_chk_ptr = (LWSEM_STRUCT_PTR) ((void *) sem_chk_ptr->NEXT);
} /* Endwhile */
}