Hello
I'm using a tower K60n512 with MQX 4.1.1 with KDS 2.0.0
I have the following configuration:
1) In Settings/Target Procession/ Float ABI = FP instruction
2) In Settings/Target Procession/ FPU Type=fpv4-sp-d16
3)in user_config.h:
#define MQXCFG_ENABLE_FP 1
#define MQX_INCLUDE_FLOATING_POINT_IO 1
4) In setings\Cross ARM C Compiler\Preprocessor:
"_AEABI_LC_CTYPE=C"
"__VFPV4__=1"
"__STRICT_ANSI__=1"
"_DEBUG=1"
In a Main task, I made following:
test1 = 16.365; test2 = test1 * 2;
So when I do a Step on line2, execution stop on an ISR (Refer to joined file)
Do you have any idea why this crash?
NB: I had a similar project bu with the Tower K70 without any crash on float calculs:smileyplain:
已解决! 转到解答。
Yes, you are right.
Your MCU has no FPU unit.
We support three different K60 twr boards and only one has FPU unit.
I suppose that you have old TWR-K60N512 or new TWR-K60D100 board. These boards are assembled by MK60N512 (old name) or MK60DN512(new name) chips.
TWR-K60F120M is assembled by MK60FN1M which contains FPU unit (“F” in part name). Chips with "D" in part name has no FPU unit.
I hope it helps you.
Have a great day,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I was TRYING to get you to do a little of your own legwork. A simple search of 'K60 floating point enable' gave a list, about the fourth of which is:
I have already found some part of code to "enable" explicitly the FPU:
; CPACR is located at address 0xE000ED88
LDR.W R0, =0xE000ED88
; Read CPACR
LDR R1, [R0]
; Set bits 20-23 to enable CP10 and CP11 coprocessors
ORR R1, R1, #(0xF << 20)
; Write back the modified value to the CPACR
STR R1, [R0]
But I don't found any explanation of this register in the RM.
I use MQX: this is not done by an OS services?
And then, why this work without any add with Tower K70?
I will test this code...
I add and call this code before float manipulation:
void vPortEnableVFP(void) { /* The FPU enable bits are in the CPACR. */ __asm volatile ( " ldr.w r0, =0xE000ED88 \n" /* CAPCR, 0xE000ED88 */ " ldr r1, [r0] \n" /* read CAPR */ " orr r1, r1, #(0xf<<20) \n" /* Enable CP10 and CP11 coprocessors */ " str r1,[r0] \n" /* store to new value back */ : /* no output */ : /* no input */ : "r0","r1" /* clobber */ );
But this not work again.:smileyconfused:
Ok,
I understand this.
But for my problem, adding lines written above don't solve my problem:smileyplain:.
And then why all work on a K70 without these line, and an equivalent project not work on K60?:smileyconfused:
MQX has a file named "not.s in \mqx\source\psp\cortex_m\core\M4\boot.s with following code:
#if MQXCFG_ENABLE_FP && PSP_HAS_FPU /* CPACR is located at address 0xE000ED88 */ LDR.W R0, =0xE000ED88 /* Read CPACR */ LDR R1, [R0] /* Set bits 20-23 to enable CP10 and CP11 coprocessors */ ORR R1, R1, #(0xF << 20) /* Write back the modified value to the CPACR */ STR R1, [R0] /* turn off fpu register stacking in exception entry */ ldr r0, =0xE000EF34 /* FPCCR */ mov r1, #0 str r1, [r0] #endif
But never execute this code.
I will check if the define ENABLE_FP and PSP_HAS_FPU are defined, but nothing line code of boot.s file are executed.
How activate this part?
Edit:
According file mqx\source\psp\cortex_m\kinetis.h, the CPU defined for the Tower K60 is (in user_config.h)MQX_CPU = BSP_CPU_MK60DN512Z
So with this CPU, the #define PSP_HAS_FPU is not define. THen I deduce my processor does not have FPU?
This will explain why this work with the K70 and not with my K60.
How know which CPU has oar hasn't FPU?
Yes, you are right.
Your MCU has no FPU unit.
We support three different K60 twr boards and only one has FPU unit.
I suppose that you have old TWR-K60N512 or new TWR-K60D100 board. These boards are assembled by MK60N512 (old name) or MK60DN512(new name) chips.
TWR-K60F120M is assembled by MK60FN1M which contains FPU unit (“F” in part name). Chips with "D" in part name has no FPU unit.
I hope it helps you.
Have a great day,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------