Hi, Changfu
Which KL25Z board you use? Freedom board? Which example project you use? USB stack V4.0.3? If you use USB stack V4.0.3 and freedom board, please change attached file to path ...\Freescale\Freescale USB Stack v4.0. \Source\Device\app\common.
Hope my reply can help you.
Best Regards
Paul
I copy your attach file to “...\Freescale\Freescale USB Stack v4.0.3 \Source\Device\app\common”, and compile again, I got error:
C:/CW_10_4_workplace/USB_HID_MOUSE_DEVICE_MQX_Lite_MKL25Z128_PEx/Generated_Code/types.h:61:25: error: conflicting types for 'boolean'
Same as “bool” and “boolean” two define
And “boolean” has two define:
Unit8
Uint32
Hi, Zhe Tian,
First appreciate your respond.
I am using KL25Z freedom board, CW10.4, and USB stack V4.03 and V4.11, and more I wand use MQX_Lite
My question is:
Can I use USB Stack with MQX_Lite?
I import example project “USB_HID_MOUSE_DEVICE_MKL25Z128_PEx”, after I try to compile it, I got many error,
I am a new for USB, so I don’t know how can I to do if the example was wrong
I am working on a new production with KL25Z, so please help me solve this problem.
Our project is a HID device connect to cell phone, I only didn’t complete USB part.
Thank you very much
Regards,
Henry ( Changfu ) Zhao