I am using a K52DN512Z on a custom board. I used the BSP Cloning Wizard (using TWR-K53N512 as a starting point) and called mine MyBSPClone.
When I moved the .wsd file into an empty CW project and built the projects, there were no problems but over 200 warnings.
My question is, when I start a new MQX4.0 project, how do I get my custom BSP to show up as one of the choices along with the TWR boards? I found the instructions on how to do this with MQX 3.8 but it appears the file structure is different in MQX 4.0
Thank you.
Gary
已解决! 转到解答。
Follow the document on the link below, New Project Wizard modification on pages 22-25:
https://community.freescale.com/message/306164#306164
In CW 10.4, the path to the Kinetis xml files is:
c:\Freescale\CW MCU v10.4\MCU\lib\wizard_data\mqx\4.0\arm\
Follow the document on the link below, New Project Wizard modification on pages 22-25:
https://community.freescale.com/message/306164#306164
In CW 10.4, the path to the Kinetis xml files is:
c:\Freescale\CW MCU v10.4\MCU\lib\wizard_data\mqx\4.0\arm\
Hi Martin,
I installed CW 10.4 and MQX 4.0.2 on my Windows 7 PC.
I used BSP Cloning Wizard to clone twrk60n512 MQX libraries for my custom board TB4, following "Getting Started with Freescale MQX BSP Cloning Wizard.pdf" help document.
The wizard generated TB4.reg and TB4.xml files in the "<MQX_4_0>\tools\CodeWarriorNPW" folder. I imported TB4.reg in Windows and copied TB4.xml in the "<CW_10_4>\MCU\lib\wizard_data\mqx\4.0\arm" folder, where the XML files for Kinetis Evaluation boards are already present.
I started CW and tried to create a new MQX project for my TB4 board, but my new board does not appear in the Kinetis board list.
How can I fix it?
Thank you.
I'm having the exact same issue. I have three custom BSPs I've cloned/developed so far, but I cannot get them to appear in the New Project Wizard. I've tried copying them to C:\Freescale\CW_MCU_v10.5\MCU\lib\wizard_data\mqx\4.0\arm, or one level above that, but after closing and restarting CW, nothing changes, I just see the eval boards. C'mon Freescale, what's the trick?
The BSP Cloning Wizard for MQX with Freescale MQX 4.0.2 generates two files to support CodeWarrior New Project Wizard for a BSP clone: .reg and .xml in c:\Freescale\Freescale_MQX_4_0\tools\CodeWarriorNPW\. The .xml file is to be located in C:\Freescale\CW_MCU_v10.5\MCU\lib\wizard_data\mqx\4.0\arm
The .reg file is for 32-bit Windows (at the moment). For a 64-bit Windows 7, we have been told the .reg file needs to be changed as shown in the below example (note the "Wow6432Node"):
Windows Registry Editor Version 5.00
[HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Freescale\Freescale MQX\4.0 newbsp]
"INSTALL_DATE"="10-09-2013"
"PACKAGE_DATE"="2013/09/10"
"PACKAGE_SIZE"="0"
"PATH"="C:\\Freescale\\Freescale_MQX_4_0"
"VERSION"="4.0.2"
Tried it, still didn't work. Running Windows 7 x64. These are my file contents:
Windows Registry Editor Version 5.00
[HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Freescale\Freescale MQX\4.0 CAM_DBU_K60F120M]
"INSTALL_DATE"="03-10-2013"
"PACKAGE_DATE"="2013/10/03"
"PACKAGE_SIZE"="0"
"PATH"="C:\\Freescale\\mqx_4.0"
"VERSION"="4.0.2"
I shut down CW 10.5, put cam_dbu_k60f120m.xml in C:\Freescale\CW_MCU_v10.5\MCU\lib\wizard_data\mqx\4.0\arm, executed cam_dbu_k60f120m_x64.reg (my hack of the original .reg file), restarted CW, and tried creating a new project... the same board families were listed (CF, CF+, and Kinetis eval boards), no listing for my custom board.
There's got to be a better way to do this. This functionality should be integrated into the BSP Cloning Wizard, instead of having us manually copy XML files and hand-install registry files.