I am trying to get the flexbus working with an 8 bit peripheral. I have CW, MQX and PE installed and working.
hardware designer, haven't written C for a long time, never used Eclipse before, or any real time OS so some things that are obvious to an experienced software person might need a little extra explanation.
I have two questions, first is getting the flexbus setup correctly, the second is about removing stuff I don't need without breaking the compile.
I have a tower k60F system wired up to some external hardware. I have successfully compiled and run the PE demo. Then I added some PE LDD components (GPIO and SPI slave) and moved the RS232 port to different pins. I can toggle the GPIOs and the RS232 port works in it's new location. I haven't tried the SPI interface yet but I expect it to work OK because the PE configuration was straightforward.
The problem is with the flexbus interface and CW / MQX / PE combo. PE says that the flexbus is configured in MQX. In init_hw.c there are the following lines:
#if PE_LDD_VERSION
__pe_initialize_hardware();
#else
_bsp_initialize_hardware();
I know it's using the pe_initialize because I edited the bsp_initialize files but it didn't have any effect. The pe code is generated so I can't edit it, but it does have a call to a user init. I found the file that calls the user function once but I can't seem to locate it again. Can someone tell me where it is so I can get the name of the function I need to write to initialize the flexbus the way I want it.
I found in other discussions that the address used for the MRAM and LCD are cachable so I should move my peripheral up to A000000 if I don't want to turn off caching. I will be using CS0 and CS1 so I have to overwrite the flexbus settings that are generated for the MRAM and LCD. I don't need the MRAM or LCD config so how do I get CW / PE to stop generating the flexbus config for them without breaking something in the compile?
The external devices are DS26521 T1 framers. I have actually managed to read the ID because the mram config was close enough for some data to come out but I know the bus isn't correct yet and the caching probably didn't help either. I am sure I can get it to work right I just need a couple pointers to the right files to edit to get the flexbus set up correctly.
Thanks,
Steve
Hi Steven,
In C:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60f120m\init_hw.c you will find the functions that initialize flexbus. These functions are
static void _bsp_flexbus_setup (void)
static void _bsp_flexbus_mram_setup (const uint32_t base_address)
The base address is provided by the linker file:
C:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60f120m\gcc_arm\intflash.ld
__EXTERNAL_MRAM_BASE = 0xA0000000;
For details about disabling code generation please see the post below:
http://mcuoneclipse.com/2012/03/23/disable-my-code-generation/
Rest regards,
Carlos
Hi Carlos:
Slow reply because I only get a bit of time now and then to look at this.
I can read and write to the device when I move it to 0xA000000 but I have yet to get it to work the way I want at 0x7000000 even if I add a call to _DCACHE_DISABLE(). I don't know if that call is in the correct place. I don't want to disable code generation because I have more PE components to add.
What I found so far:
in init_hw.c, __pe_initialize_hardware() is called.
That function is found in BSP files -> generated code -> CPU.c
Then to add user code in __pe_initialize_hardware, in the processor expert components view, select the processor, then in the component inspector select the "build options" tab and there is a place to enter a few lines of text before or after the generated __pe_initialize_hardware() code. This all seems to work but I don't think I need to add any code there. I haven't figured out how to get the flexbus working in the cachable address space.
Where should the call to _DCACHE_DISABLE() go?
The reference I saw to using it referred to putting it at the start of main, but that doesn't apply here since I'm using MQX so all I have is the tasks created based on the example hello project. What would be the correct way to disable caching when using MQX and processor expert?
Thanks,
Steve