Hi, I recently installed MQX 3.8.1 and I'm testing the 52259EVB HVAC demo included with the project. Everything works OK when I set
DEMOCFG_USE_POOLS= 0 in hvac.h. I have 1MB of extended memory installed and verified that it works by reading and writing it from the debugger shell. When I set DEMOCFG_ENABLE_KLOG =1, I can read the kernel log via the CodeWarrior 10 TAD, so it appears to be working OK. When I set DEMOCFG_USE_POOLS=1, the network stops responding to pings. The TAD "Lightweight Memory pools" and "Check for Errors" screens show the pools above 0x10000600, and no errors.
I'm using the default "small_ram_config.h" in user_config.h and override the following options:
#define MQX_USE_LOGS 1
#define MQX_USE_IDLE_TASK 1
#define MQX_USE_SEMAPHORES 1
#define MQX_USE_TIMER 1
#define MQX_USE_SW_WATCHDOGS 1
#define MQX_KERNEL_LOGGING 1
#define HTTPD_DBG_LEV 2 // http debug info level ( 0 - 4 )
I also set the following in hvac.h:
#define DEMOCFG_ENABLE_SERIAL_SHELL 1 /* enable shell task for serial console */
#define DEMOCFG_ENABLE_SWITCH_TASK 0 /* enable button sensing task (otherwise keys are polled) */
#define DEMOCFG_ENABLE_AUTO_LOGGING 1 /* enable logging to serial console (or USB drive) */
#define DEMOCFG_ENABLE_USB_FILESYSTEM 0 /* enable USB mass storage */
#define DEMOCFG_ENABLE_RTCS 1 /* enable RTCS operation */
#define DEMOCFG_ENABLE_FTP_SERVER 0 /* enable ftp server */
#define DEMOCFG_ENABLE_TELNET_SERVER 0 /* enable telnet server */
#define DEMOCFG_ENABLE_WEBSERVER 1 /* enable web server */
#define DEMOCFG_ENABLE_KLOG 1 /* enable kernel logging */
#define DEMOCFG_USE_POOLS 1 /* enable external memory pools for USB and RTCS */
#define DEMOCFG_USE_WIFI 0 /* use WiFi Interface */
Any ideas?
Thanks, John Reynolds