I've been trying to initialize 2 separate gpio pins to have 2 separate interrupt handlers, however they seem to only be linked to the 2nd handler i initialize. Is there some hardware restriction I am missing where 2 pins of the same port must share 1 interrupt hander? I am seeing that although they are different pins, that the lwgpio_int_get_vector function is returning the same value for both.
LWGPIO_STRUCT column_1;
LWGPIO_STRUCT column_2;
lwgpio_init(&column_1, (GPIO_PORT_B | GPIO_PIN17), LWGPIO_DIR_INPUT, LWGPIO_VALUE_NOCHANGE);
lwgpio_set_functionality(&column_1, 1);
lwgpio_set_attribute(&column_1, LWGPIO_ATTR_PULL_DOWN, LWGPIO_AVAL_ENABLE);
lwgpio_int_init(&column_1, LWGPIO_INT_MODE_RISING);
_int_install_isr(lwgpio_int_get_vector(&column_1), column_1_button_pressed_function, (void *) &column_1);
_bsp_int_init(lwgpio_int_get_vector(&column_1), 3, 0, TRUE);
lwgpio_int_enable(&column_1, TRUE);
lwgpio_init(&column_2, (GPIO_PORT_B | GPIO_PIN18), LWGPIO_DIR_INPUT, LWGPIO_VALUE_NOCHANGE);
lwgpio_set_functionality(&column_2, 1);
lwgpio_set_attribute(&column_2, LWGPIO_ATTR_PULL_DOWN, LWGPIO_AVAL_ENABLE);
lwgpio_int_init(&column_2, LWGPIO_INT_MODE_RISING);
_int_install_isr(lwgpio_int_get_vector(&column_2), column_2_button_pressed_function, (void *) &column_2);
_bsp_int_init(lwgpio_int_get_vector(&column_2), 3, 0, TRUE);
lwgpio_int_enable(&column_2, TRUE);
vector_value = lwgpio_int_get_vector(&column_1);
vector_value = lwgpio_int_get_vector(&column_2);
void column_1_button_pressed_function(void *pin)
{
printf("1\r\n");
lwgpio_int_clear_flag((LWGPIO_STRUCT_PTR) pin);
}
void column_2_button_pressed_function(void *pin)
{
printf("2\r\n");
lwgpio_int_clear_flag((LWGPIO_STRUCT_PTR) pin);
}
解決済! 解決策の投稿を見る。
Hello albert calpito,
you almost answered your question. I would recommend read NVIC part in a reference manual. Each port has own interrupt handler which indicates that your two buttons on PORTB share same ISR.
There is even here a discussion about it and how they solved an identification which button was pushed in ISR.
Regards,
c0170
Hello albert calpito,
you almost answered your question. I would recommend read NVIC part in a reference manual. Each port has own interrupt handler which indicates that your two buttons on PORTB share same ISR.
There is even here a discussion about it and how they solved an identification which button was pushed in ISR.
Regards,
c0170
Hi I am having similar issue, can you please point to the discussion of how to resolve it.
Thanks
Nikhil
I have just responded to the thread with some c and h files to solve this issue.
Thank you,
Sincerely,
Albert Calpito
Ayantra
47873 Fremont Blvd,
Fremont. CA 94538
<http://www.ayantra.com> www.ayantra.com
510-623-7526 Office
510-552-4399 Cell
510-623-7839
Hi Albert
Many thanks for your sharing.
But still need your help.
I got an issue on lwevent settings.
I have assign a lwevent to a gpio.
But the handler task can not receive the lwevent even if interrupt occur and set the event.
Hi Albert
Sorry for bother you.
I fix this issue just now.
I find that missing some address map code in the "register_gpio_file".
It is works fine now.
Many thanks for your effort again.
Thanks Albert for your info, I fixed it, it was error in my code. I was not clearing the correct interrupt flag.
Nikhil
Hello Nikhil,
Please see the attached files. I've written an init function that will map interrupt events for the gpio's to their specific interrupt handlers. The interrupt handlers will set the event that was specified in the init structure.
I've tested this for a few gpios at a time, and basic functionality seems to be working.