the ethernet project for DSRC communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the ethernet project for DSRC communication

678件の閲覧回数
961271210
Contributor I

Anyone has the ethernet example project or ethernet head files which can be use in the DSRC communication between two mpc5748g?Or which ethernet api can be used if I want to construct DSRC communication between two mpc5748g?

タグ(3)
0 件の賞賛
返信
1 返信

611件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

seems we have nothing for the DSRC on the MPC5748G.

See more in DSRC Safety Modem | NXP 

BR, Petr

0 件の賞賛
返信