Q1: when I write Run=0 and then write Run=1, will flexPWM generate Local Reload Signal?
Q2: SUBn_CTRL1[PRSC], SUBn_INIT and SUBn_VALx have buffers. I want to ask when I configure these registers the first time after reset, where did I write to? the outer buffers or the inner?
Q3: (fellow Q2) if the answer is the outer buffers, what is happening when I set Run=1?
As I think it will first generate local reload signal, secondly reload the buffers to the inner, at last run as I have configured. Is that correct? If no what is the right process?
Q4: in my program I use flexpwm0 pwmx0 trigger ctu0, flexpwm1 pwmx0 trigger ctu1, and ctu0&ctu1 trigger ADC0-3, so I configure flexpwm1 use EXT_SYNC to Initialize itself. The code is as follows:
FlexPWM1.SUB[0].CTRL2.B.INIT_SEL = 3; /* 11 = EXT_SYNC causes initialization */
where the ext_sync signal to flexpwm1 is the master reload signal of flexpwm0.
A strange thing I found is that at the first cycle of flexpwm1, flexpwm1 seems cann’t trigger ctu1. After the first cycle, the flexpwm1 trigger ctu1 well. i want know why?
PS: when I configure flexpwm1 INIT_SEL=0 (local sync cause initilation), it will be ok.
Q5: Another thing I found is that under this condition( flexpwm1 INIT_SEL=3), it seems that when I set flexpwm0 Run=0 and then set flexpwm0 Run=1, it will reset flexpwm1 counter register((FlexPWM_SUBn_CNT) , does that mean a master reload signal has generated?
Thank you very much!
Problem solved!(By Doctor Gong)
Give a record here:
原因是FlexPWM0产生的reload信号(用于同步FlexPWM1)在一个采样循环内周期不一致,即同步运行后的第一个cycle中reload周期偏小。这是因为在FlexPWM0从RUN=0倒RUN=1的过程中,COUNTER没有初始化。
改进如下:
在PWM初始化函数void PWM_Init(uint16_t PWMFre, uint8_t nbPWM, uint8_t nCH)中,增加如下代码即可:
p_PWM->SUB[nCH].CTRL2.B.FRCEN = 1;
p_PWM->SUB[nCH].CTRL2.B.FORCE_SEL = 2;
Hi,
A1) upon reset yes. Otherwise it depends on the counter value
A2) to the set of outer buffer
A3) you are correct
A4) try to measure PWMx signal with a scope, and see what happens on it in first period.
Within CTU you can select rising or falling edge of PWMX for MSR trigger. Did you test both options?
A5) yes, Master reload was generated.
BR, Petr
i have measured the flexpwm1_pwmx0, ctu0trigout, ctu1trigout( flexpwm0_pwmx0 not measured because the limit of the board)
both pics are Ch1: flexpwm1_pwmx0 Ch2: ctu0trigout Ch3:ctu1trigout
this is the first pic, it seems that flexpwm1's first cycle didn't wor well. my configuration is that the period is 80us and val0=val1/2 (both pwm0&1 are the same)
the second pic i set flexpwm1 INIT_SEL=0 (local sync cause initilation),
p_PWM->SUB[nCH].CTRL2.B.INIT_SEL = 3; /* 11 = EXT_SYNC causes initialization */
----->p_PWM->SUB[nCH].CTRL2.B.INIT_SEL = 0; /* 11 = EXT_SYNC causes initialization */
Another strange thing is i have set the etimer to count 24 triggers(as pic below), but it seems only 12 trigger will cause the interrupt, i have checked the settings and find no reason? can you help me for that, thank you very much!
PS: my program process is :
flexpwm0&1 trig ctu0&1
ctu0&1 trig adc&etimer
dma move adc data to ram and etimer count trig number and when number satisfy then stop flexpwm0&1
cycle again
the source code has attached.
if i choose FlexPWM_x OUT_TRIG0_0 as CTU_x_TGSISR source(in the previous experiment FlexPWM_x PWMX0 was chosed as the CTU_x_TGSISR source) then the first cycle will trigger ok. But the pwmx0 still seems do not work well on the first cycle. you can see the pic below
Hi,
The first PWMX1 cycle is missed because there is no compare with VAL1 at FlexPWM1 module.
Try to use below code to start and stop PWMs. Note the FORCE is enabled, so add below line in PWM init
p_PWM->SUB[nCH].CTRL2.B.FRCEN = 1; /* PWM Force Initialization Enable */
void Samp_Start(void)
{
uint32_t i;
DMA_Req_Enable();
ETIMER_0.ENBL.R = 0x0001; /* Enable eTimer[0].[0]*/
FlexPWM_1.MCTRL.B.RUN = 1u; // start FlexPWM1 first so it can be synchronized by FlexPWM0
FlexPWM_0.MCTRL.B.RUN = 1u; /* Run PWM*/
}
void Samp_Stop(void)
{
uint16_t temp,i;
FlexPWM_0.MCTRL.B.RUN = 0; /* Stop All Channels*/
FlexPWM_1.MCTRL.B.RUN = 0;
temp = FlexPWM_0.SUB[0].VAL1.R; // save current VAL1 value
// update FlexPWM0 VAL1 immediately so the Master reload can be generated at FlexPWM0 counter start
FlexPWM_0.SUB[0].CTRL1.B.LDMOD = 1;
FlexPWM_0.SUB[0].VAL1.R = 0;
FlexPWM_0.MCTRL.B.LDOK = 1;
while(FlexPWM_0.MCTRL.B.LDOK){}; // wait till load is done
FlexPWM_0.SUB[0].CTRL2.B.FORCE = 1; // reinit FlexPWM counter
FlexPWM_1.SUB[0].CTRL2.B.FORCE = 1;
// update FlexPWM0 VAL1 buffer with saved value, will be loaded on first reload
FlexPWM_0.SUB[0].CTRL1.B.LDMOD = 0;
FlexPWM_0.SUB[0].VAL1.R = temp;
FlexPWM_0.MCTRL.B.LDOK = 1;
}
Seems this help, but it would be better to use PWMA or PWMB instead of PWMX as the edge will not be lost.
For the eTimer trigger count issue; this looks really strange, let me some time to check this too.
BR, Petr
i want to know what does that mean"no compare with VAL1 at FlexPWM1 module", why no compare?
Thank you very much!
For a eTimer counting, this is because you have measured CTU_EXT_OUT signal, which is toggled at each CTU trigger.
However the CTU’s ETIMER0_TRG signal is just single pulse (1 CTU clock) at each CTU trigger, so you have each time 2 edges on single CTU_EXT_OUT toggle.
BR, Petr
Thank you Peter, Thank you very much!
Because on subsequent PWM start both modules are not synchronized. There is no reload at PWM0 start at this point.
And because the PWMs are not started at the same time, in your code PWM0 starts first, the PWM0 cycle (VAL1 compare) ends sooner then it is on PWM1. Master reload is issued on this end of PWM0 cycle. PWM1 counter reinits, but there was no VAL1 compare in fact, that’s why there is missing falling edge. From now both PWMs are synchronized , but you do not see rising edge as the output is high still. You can see falling edge on second PWM cycle.
If the code I sent does not work, try to add some delay between PWM1 and PWM0 start.
Still I think a usage of PWMA or PWMB leads brings better functionality, but it depends if your application could use that.
BR, Petr
i have tried your seetings, as you can see below
but it seems did not ok. you can see there are some miss(blue part)