Hi,
I am configuring etpu_a channel 0 for pwm generation.
I have downloaded the etpu pwm apis, however in function fs_etpu_pwm_init
int32_t fs_etpu_pwm_init( uint8_t channel, uint8_t priority, uint32_t freq,
uint16_t duty, uint8_t polarity, uint8_t timebase, uint32_t timebase_freq)
{
uint32_t *pba; /* parameter base address for channel */
uint32_t chan_period;
......
/* write hsr to start channel running */
eTPU->CHAN[channel].HSRR.R = FS_ETPU_PWM_INIT;
return(0);
}
not able to write anything in HSRR register.
I am using basic etpu generation code and example only.
Any suggestion???
Regards
Vrushali
I further debug the code and found that
Before writing CR and SCR register, We can update HSRR register,
After cofniguring CR and SCR register, value of HSRR is changed by 0 and non-writable mode.
eTPU->CHAN[channel].HSRR.R = FS_ETPU_PWM_INIT;
/* write channel configuration register */
eTPU->CHAN[channel].CR.R = (priority << 28) +
(FS_ETPU_PWM_TABLE_SELECT << 24) +
(FS_ETPU_PWM_FUNCTION_NUMBER << 16) +
(((uint32_t)pba - fs_etpu_data_ram_start)>>3);
/* write FM (function mode) bits */
eTPU->CHAN[channel].SCR.R = (timebase << 1) + polarity;