problem about MPC5746R_MCAL4_0_RTM_1_0_2 license

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem about MPC5746R_MCAL4_0_RTM_1_0_2 license

1,496 Views
pwok2004
Contributor I

I use EB tresos 24.1 and  mpc5746r_ MCAL4_ 0_ RTM_ 1_ 0_ 2 developed projects,and

MPC5746R_ MCAL4_ 0_ RTM_ 1_ 0_ 2. Use the free license of NXP official website.

When I configuring official routines(MPC5746R_MCAL4_0_RTM_1_0_2_Sample_Application)

Report error about license,such as:

  

Failed to retrieve crypto key data from license feature "EB_TS_MOD_SGNNXP".

Failed to retrieve vendor string: feature "EB_TS_MOD_SGNNXP" not licensed.

Failed to retrieve crypto key data from license feature "EB_TS_MOD_SGNNXP".

pastedImage_8.png

in addition:

         when I creat a new project, some module need license ,and can’t add to project,

such as Base_TS_T2D34M10I2R0、,but others do not.

What's the problem? Please help, thank you!

pastedImage_7.png

0 Kudos
Reply
3 Replies

1,451 Views
namnguyenviet
NXP Employee
NXP Employee

Hello pwok2004@163.com‌,

Please try with the EB version validated in the release: "EB tresos Studio 14.2.1 b140128-1223". I tried with that version and I was able to add the Base module and generate the code successfully.

Best Regards,

Nam

0 Kudos
Reply

1,451 Views
pwok2004
Contributor I

Thank you very much. The problem has been solved according to your suggestion.

Thanks again!

0 Kudos
Reply

798 Views
lulu_zhang
Contributor I
I also ran into this problem, how did you solve it?
0 Kudos
Reply