mpc5746r VDD_HV_IO_MAIN spec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc5746r VDD_HV_IO_MAIN spec

729 Views
alistairhill
Contributor II

The data sheet for the MPC5746R Rev 4 specifies VDD_HV_IO_MAIN as 3.5V to 5.5V but note 7 of Table 3 states "The pad are operative till 3.0V full performance. The IRC oscillator is supplied by this pin and it is setting the min voltage limit" implying that the IO is perfectly good with VDD_HV_IO_MAIN=3.3V nominal which would be much more convenient for my application.

The limitation appears to be the internal RC oscillator so is there a work round that would allow me to use 3.3V given that the RC oscillator is needed for startup and some of the peripherals, I am using an external clock

Thanks

Labels (1)
0 Kudos
1 Reply

573 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there's no workaround. VDD_HV_IO_MAIN mus be 3.5V at least, typically 5V.

LVD_IO circuit does not allow us to operate this supply rail at 3.3V:

pastedImage_0.png

Regards,

Lukas

0 Kudos