Dear Sir,
According to AN4234 source code project readme.txt, I can run the script in cygwin to generate M1~M5.
I have installed cygwin and entered tcsh shell.
I can run the script:
"source create_M1_to_M5 2FF8B03C5C5405465A9C94BD2D863279 00000000000000000000000000000000 FFFFFFFFFFFFFFFFFFFFFFFFFFFFFF 4 4 0000001 00"
But K1, K2, M2... cannot be generated and is empty. Looks like the four exe in bin directory cannot be executed.
"AES_CMAC_CMD.exe AES_ENC_CBC_CMD.exe AES_ENC_ECB_CMD.exe AES_MP_KDF_CMD.exe"
Do you have any comments or suggestions on what I need take into consideration?
Regards,
Jason Yang
Hi Jason,
do you use 32bit Windows or 64bit? I can remember I tested it on 64bit system and it didn't work correctly. Try it on 32bit system if possible. It worked as expected on my side.
Regards,
Lukas